PE on CW 10.2 Special Edition

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PE on CW 10.2 Special Edition

2,426 次查看
emb_developer
Contributor I

I have downloaded CW 10.2 Eclipse Special Edition. I didn't see PE and device inilization on menus. Has it been removed? 

标签 (1)
标记 (1)
0 项奖励
回复
9 回复数

1,580 次查看
ProcessorExpert
Senior Contributor III

Hello,

 

could you please provide more details? What MCU are you targeting?

 

best regards
Vojtech Filip
Processor Expert Support Team


0 项奖励
回复

1,580 次查看
emb_developer
Contributor I

Thank you for your interest. I tried it for both HCS08 and 56F82xx but PE menu is not available in IDE. Also when creating new project there is no device initilaziton selection. I have CW10.1 special editon installed also. It works properly excepting PE License error for HCS08 MCUs. What's wrong with these IDEs?   

0 项奖励
回复

1,580 次查看
BlackNight
NXP Employee
NXP Employee

Hello,

it might be an installer problem as I have seen a similar problem on another machine.

 

Could you check if following folder is installed on your system (start of path depends on your installation folder):

C:\Freescale\CW MCU v10.2\MCU\ProcessorExpert

 

Next, could you check if you have any com.freescale.processorexpert.* plugins present in

C:\Freescale\CW MCU v10.2\eclipse\plugins

 

As for diagnostics: could you attach the fillowing file to this thread:

eclipse\configuration\org.eclipse.equinox.simpleconfigurator\bundles.info

 

And: what kind of machine are you using? Windows 7 32bit? or 64bit?

 

Thanks,

BK

0 项奖励
回复

1,580 次查看
emb_developer
Contributor I

The OS is WinXP.

 

I have reinstalled CW now it appears on menus. But this time when I click generate code it says "Cannot generate - no active project is selected in project panel". If I choose PE when creating project and check add main.c to project, main.c is not created. Similarly for device initialization no mcu_init.c/h file is created.  And in the target cpu window it says "no cpu selected". The CW 10.2 special editon contains lots of bugs.

 

0 项奖励
回复

1,580 次查看
BlackNight
NXP Employee
NXP Employee

Hello,

Looks like either you do not have a Processor Expert project selected, or you have no Processor Expert project at all in your workspace.

Maybe have a look here:

http://mcuoneclipse.wordpress.com/2012/03/09/quickstart-for-processor-expert-in-eclipse/

 

Hope this helps,

BK

 

0 项奖励
回复

1,580 次查看
emb_developer
Contributor I

Here is console window output:

 

09.Mar.2012 14:49:42 Starting Processor Expert service
System directory = C:\Freescale\CW MCU v10.2\MCU\ProcessorExpert
User working directory = C:\Documents and Settings\All Users\Application Data\Processor Expert\CWMCU_PE5_00
Internal cache directory = C:\Documents and Settings\All Users\Application Data\Processor Expert\PECache\4fa5ce92
09.Mar.2012 14:49:47 FAILED starting Processor Expert service
09.Mar.2012 14:54:59 Could not open project L/test_PE/ProcessorExpert.pe. Processor Expert service is not initiated yet.
09.Mar.2012 14:55:58 Could not open project L/test_PE/ProcessorExpert.pe. Processor Expert service is not initiated yet.

 

Why does PE service fail? 

0 项奖励
回复

1,580 次查看
emb_developer
Contributor I

I have tried CW10.2 on an another machine similarly it doesn't work because of the PE fail. Need help.

0 项奖励
回复

1,580 次查看
emb_developer
Contributor I

No solution to that problem?

0 项奖励
回复

1,580 次查看
ProcessorExpert
Senior Contributor III

Hello,

 

please enter service-request:

 

https://www.freescale.com/webapp/servicerequest.create_SR.framework

 

best regards
Vojtech Filip
Processor Expert Support Team

0 项奖励
回复