what is my boards ip address

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

what is my boards ip address

834 Views
ssssss
Contributor II

hi

i have a mpc8568 eval board.

i need to know my board's ip but i didn't find it in any doc . what should i do?

(i couldn't boot linux on it,so i can't use linux to find it )

hossein

Tags (2)
0 Kudos
1 Reply

660 Views
alexander_yakov
NXP Employee
NXP Employee

The IP address to the board is assigned by Linux. If you do not have Linux on your board than you can not connect to this board externally.

Do you have working U-boot on your board? If yes than you can connect the to board to the PC via serial console cable and burn Linux image using U-boot commands

If you do not have working U-boot, than you need debug probe to flash the onboard flash.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos