base address of the page 5 of ds2155 chip

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

base address of the page 5 of ds2155 chip

Jump to solution
629 Views
dongpolu
Contributor I

hello!

Excuse me:

What is the base address of the page 5 of ds2155 chip(MPC_SOM_LCS2#) corresponding in the schematic diagram (Freescale FREESCALE_MPC830x_CARRIER.pdf )。

Thanks!

0 Kudos
1 Solution
431 Views
alexander_yakov
NXP Employee
NXP Employee

Memory map is not fixed - every chip select line is configurable.

For CS2 line please configure OR2 and BR2 register pair.

Base address is configured in BR2

There is no default base address value.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
1 Reply
432 Views
alexander_yakov
NXP Employee
NXP Employee

Memory map is not fixed - every chip select line is configurable.

For CS2 line please configure OR2 and BR2 register pair.

Base address is configured in BR2

There is no default base address value.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos