sbc:FS2633D
1. what is the default state of LDO and GPIO? it can be configed in OTP mode, In non-OTP mode(for example normal mode), what is the voltage of LDO pin(3.3V/5V), GPIO1/2 is input or output?
2. since OTP mode should not be used in production applications, usage of LDO and GPIO is limited?
Solved! Go to Solution.
Hi Zhou,
Once you burn an OTP configuration permanently into the fuses, the SBC powers up with OTP configuration burned.
For example if VLDO1_OTP = 0, the LDO1 voltage in normal mode will be 3.3V. If VLDO1_OTP = 1, the LDO1 voltage in normal mode will be 5V.
GPIO1 configuration is selectable using the GPIO1STAGE_OTP[1:0] bits.
BR, Tomas
Hi Zhou,
Once you burn an OTP configuration permanently into the fuses, the SBC powers up with OTP configuration burned.
For example if VLDO1_OTP = 0, the LDO1 voltage in normal mode will be 3.3V. If VLDO1_OTP = 1, the LDO1 voltage in normal mode will be 5V.
GPIO1 configuration is selectable using the GPIO1STAGE_OTP[1:0] bits.
BR, Tomas