Power Supply for LS1046

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Power Supply for LS1046

970件の閲覧回数
Ellu24
Contributor III

I am trying to bring up a board using LS1046 and using a design similar to freeway board. I am using PF8100 and LTC7150 for multioutput voltages and VDD respectively. I am using programmable DC power supply for giving 3.3V,3 A and 12V,1.8A as input and not observing the expected voltages. Please find the attachment to see the measured and expected voltages. Please help me to resolve the problem.

Is there any software to simulate PF8100?

 

Thanks in advance 

0 件の賞賛
5 返答(返信)

952件の閲覧回数
Ellu24
Contributor III

Thank you very much for your advice.

I will do as per your recommendations and let you know the outcome. Is there any software that we can simulate PF8100 and observe the waveforms? Is there any reason for the unexpected voltages?

 

Thanks in advance 

0 件の賞賛

944件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

No more the simulation model for this part.

Lots of reasons can lead to the error output,for example mistake on mount components/mistake for select regulator components/etcs.

0 件の賞賛

963件の閲覧回数
Ellu24
Contributor III

Thank you very much for your prompt response. I am testing the power supply with the complete board, so that I hope each channel has load. Or please recommend me on adding load on each channel.

0 件の賞賛

962件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

You can try to add external 500mA on such as 2.5V output channel, then test again.

0 件の賞賛

965件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Did you add the load on each channel? If not please add load to test again.

 

0 件の賞賛