PF1510 taking power from VSYS?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PF1510 taking power from VSYS?

ソリューションへジャンプ
1,713件の閲覧回数
MT
NXP Employee
NXP Employee

A customer wants to power some LEDs from VSYS.

1) Is it OK to do this?

2) I assume the max current they could take would be the current taken would be dictated by the current limit setting for the Front-end LDO minus the current taken from the LDO/Switchers on the PF1510.

Thanks

Mark

ラベル(2)
0 件の賞賛
1 解決策
1,706件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi Mark,

 

Yes, you can power some LEDs from VSYS power rail from the PF1510.

 

You are correct, the max current they could take is dictated by the current limit setting for the Front-end LDO minus the current taken from the LDO/Switchers on the PF1510.

 

Regards,

Jose Reyes

元の投稿で解決策を見る

0 件の賞賛
2 返答(返信)
1,707件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi Mark,

 

Yes, you can power some LEDs from VSYS power rail from the PF1510.

 

You are correct, the max current they could take is dictated by the current limit setting for the Front-end LDO minus the current taken from the LDO/Switchers on the PF1510.

 

Regards,

Jose Reyes

0 件の賞賛
1,211件の閲覧回数
Sadatan123
Contributor I

Also Can we connect 5V to Vin of PF1510 and use Vsys to power input of all the switchers and LDO of  PMIC and also use Vsys to provide some pull ups on the boards?

0 件の賞賛