MC33771 SPI

キャンセル
次の結果を表示 
次の代わりに検索 
もしかして: 

MC33771 SPI

265件の閲覧回数
mohamed-moustafa
Contributor I

How can i know SPI commands to control PGA or IC at all ?

0 件の賞賛
2 返答(返信)

253件の閲覧回数
mohamed-moustafa
Contributor I

I cannot access those files 
where I have no response on my NDA request.

What should I do?

 

0 件の賞賛

255件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Mohamed,

The setting of the PGA gain in manual or automatic mode can be performed by configuring ADC_CFG[PGA_GAIN] register (0x06).

ADC_CFG.JPG

The setting of the PGA gain in automatic mode will also be performed by the automatic gain control. Automatic gain control allows the device to obtain the most appropriate gain setting for the amplifier input signal level. In automatic gain control mode, the conversion result is digitally compared with internally programmed thresholds.

Figure 14.JPG

You might find useful information about programming/setting the MC33771 in the AN12084 (MC3371/MC33772 Programming Guide) which is available on the product website under Secure Files requiring an NDA:

AN.JPG

In the Software section under Secure Files is also available complete BCC Software Driver:

Driver.JPG

Best regards,

Tomas

0 件の賞賛