Hi NXP experts,
for the shake of simplicity in the current stage of our project, we want to replace the FS8530 PMIC by the VR5500 PMIC so that the functional safety aspects (e.g. watchdog feature) need not to be considered right now.
And the question is:
Are the FS8530 PMIC and the VR5500 PMIC 100% compatible except for functional safety features? I.e.
Thanks very much for your support.
BL
Solved! Go to Solution.
Do you also have information regarding the following two points ?
1:Regulator outputs compatible ?
[gw]Regulators are compatible.
2:and Design compatible ?
[gw]VR5500 doesn't have FCCU and FS8530 has 4 channels of VMONx but VR500 onlh has one channel.
Please see below picture I attached for FS85/VR5500,red circle are the different points:
Hi Guoweisun,
thanks very much for the information about the Pin-compatible.
Do you also have information regarding the following two points ?
Thanks,
BL
Do you also have information regarding the following two points ?
1:Regulator outputs compatible ?
[gw]Regulators are compatible.
2:and Design compatible ?
[gw]VR5500 doesn't have FCCU and FS8530 has 4 channels of VMONx but VR500 onlh has one channel.