p2020rdb-pca PCIe does not recognize devices

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

p2020rdb-pca PCIe does not recognize devices

ソリューションへジャンプ
3,831件の閲覧回数
ymha07
Contributor II

Hi, 

I'm trying to construct a wireless communication network using the p2020rdb-pca.

After installing wlan cards using the PCIe interface on the p2020rdb-pca, I used a command 'lspci' and
got the following messages, which imply "the wlan cards are not recognized".

--- Messages ---
root@p2020rdb:~# lspci

0000:00:00.0 PCI bridge: Freescale Semiconductor Inc P2020E (rev 21)

0000:01:00.0 Mass storage controller: Silicon Image, Inc. SiI 3132 Serial ATA Raid II Controller (rev 01)

0001:02:00.0 PCI bridge: Freescale Semiconductor Inc P2020E (rev 21)

---------

I tried to configure the Linux kernel like the belows and got the same result.

Bus options --->
[*] PCI Express Port Bus support
[*]     Root Port Advanced Error Reporting support
[*] PCI Express ASPM control

There was no result of recognizing the wlan cards.
How can I solve this problem? 

0 件の賞賛
1 解決策
3,809件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please try SW2[7]=ON

元の投稿で解決策を見る

4 返答(返信)
3,825件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please provide additional information:

1) U-Boot booting log text

2) photo of the RDB board with installed PCIe card

3) positions of all on-board switches

0 件の賞賛
3,815件の閲覧回数
ymha07
Contributor II

Hi, thanks for the fast reply.

The attached files include a booting log text, photos of the RDB board with PCIe cards and on-board switches.

If I didn't attach any files in need, please let me know.

Thank you in advance for your help.

 

 

0 件の賞賛
3,810件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please try SW2[7]=ON

3,800件の閲覧回数
ymha07
Contributor II

It works ! The below is the message I got after it.

Thanks for your help!

root@p2020rdb:~# lspci

0000:00:00.0 PCI bridge: Freescale Semiconductor Inc P2020E (rev 21)

0000:01:00.0 PCI bridge: ASMedia Technology Inc. ASM1083/1085 PCIe to PCI Bridge (rev 03)

0000:02:00.0 Network controller: Cisco Aironet Wireless Communications 350 series 802.11b Wireless LAN Adapter (rev 01)

0001:03:00.0 PCI bridge: Freescale Semiconductor Inc P2020E (rev 21)

root@p2020rdb:~# iwconfig

eth3      IEEE 802.11-DS  ESSID:""  

          Mode:Managed  Frequency:2.412 GHz  Access Point: Not-Associated   

          Bit Rate:0 kb/s   Tx-Power=20 dBm   Sensitivity=0/65535  

          Retry limit:16   RTS thr:off   Fragment thr:off

          Encryption key:off

          Power Management:off

          Link Quality=0/100  Signal level=-110 dBm  Noise level=0 dBm

          Rx invalid nwid:0  Rx invalid crypt:0  Rx invalid frag:0

          Tx excessive retries:0  Invalid misc:0   Missed beacon:0

 

wifi0     IEEE 802.11-DS  ESSID:""  

          Mode:Managed  Frequency:2.412 GHz  Access Point: Not-Associated   

          Bit Rate:0 kb/s   Tx-Power=20 dBm   Sensitivity=0/65535  

          Retry limit:16   RTS thr:off   Fragment thr:off

          Encryption key:off

          Power Management:off

          Link Quality=0/100  Signal level=-110 dBm  Noise level=0 dBm

          Rx invalid nwid:0  Rx invalid crypt:0  Rx invalid frag:0

          Tx excessive retries:0  Invalid misc:0   Missed beacon:0

 

lo        no wireless extensions.

 

eth2      no wireless extensions.

 

tunl0     no wireless extensions.

 

eth1      no wireless extensions.

 

sit0      no wireless extensions.

 

dummy0    no wireless extensions.

 

eth0      no wireless extensions.

 

0 件の賞賛