hello, I am using P1023 and my phy is AR8035. the schemitic was designed refered to p1023rdb. I can boot linux normally but some problem about eth0 . When I put ifconfig eth0 up, it always :ifconfig: SIOCGIFFLAGS: No such device. You will found further information in attachement. I connect phy-AR8035 int signal to IRQ0 with correct pull-up.In addtion, the eth1 was not used and I test eth0 in uboot and the result is fine. So , I think some incorrrect settings about eth0 may be wrong in my dts.could someone check the dts for me and tell me how to modify it? thank you!
Original Attachment has been moved to: eth0_dts.rar
It looks like that your .dts file is incorrect for this PHY.
Look at the following pages:
http://man7.org/linux/man-pages/man7/netdevice.7.html
http://stackoverflow.com/questions/5308090/set-ip-address-using-siocsifaddr-ioctl
https://lkml.org/lkml/2017/2/3/396
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------