Where is the hv.dts file in Freescale SDK 1.6 for P4080DS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Where is the hv.dts file in Freescale SDK 1.6 for P4080DS

ソリューションへジャンプ
1,392件の閲覧回数
peterzheng
Contributor II

Hi,

I was trying to create 8 partitions on P4080DS using hypervisor.  I was following the documentation provided by Yiping.

https://community.freescale.com/docs/DOC-102249

However, I have trouble locate the hv.dts file. Could you help me with this issue? where is this file in the SDK after uncompress the ISO?

Thanks,

Peter Zheng

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
1,023件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hi,

Please check in attached hv-cfg-fsl-sdk-v1.6.tar.gz for SDK, under the path /p4080ds/R_PPSXX_0xe/hv-2p-Lnx-Lnx/hv.dts.

Also you can download from below for SDK1.6:

sdk/hv-cfg.git - Freescale PowerPC Hypervisor Config Tree

root/p4080ds/R_PPSXX_0xe/hv-2p-lnx-lnx/hv.dts

Is this what you want?


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
1,024件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hi,

Please check in attached hv-cfg-fsl-sdk-v1.6.tar.gz for SDK, under the path /p4080ds/R_PPSXX_0xe/hv-2p-Lnx-Lnx/hv.dts.

Also you can download from below for SDK1.6:

sdk/hv-cfg.git - Freescale PowerPC Hypervisor Config Tree

root/p4080ds/R_PPSXX_0xe/hv-2p-lnx-lnx/hv.dts

Is this what you want?


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,023件の閲覧回数
peterzheng
Contributor II

Hi Lunmin,

Thank you for your help. Could you help me take a look at another problem?

how to create 8 partitions using hypervisor in P4080DS

Thanks & Regards,

Peter Zheng

0 件の賞賛
返信
1,023件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hi,

Sure, I'll have a look soon later.

Regards

Lunmin

0 件の賞賛
返信
1,023件の閲覧回数
peterzheng
Contributor II

Hi Lunmin,

I was pointing you to the wrong question. Sorry about that. Can you take a look at this particular question?

How to partition the L3 Cacahe of P4080 using CodeWarrior?

Thank you very much for your time and help!

Regards,

Peter

0 件の賞賛
返信