Hi I'm working with a custom board based off of the P1010RDB. We are booting from NAND and are using Micron MT29F8G08ABABA as a replacement NAND. I can program the nand using jtag and uboot recognizes the NAND, after some minor changes. Uboot successfully boots to the command prompt. During boot "Bad block table not found for chip 0 No space left to write bad block table" is displayed and I cannot write to the nand chip from u-boot to save the environment or program new u-boot. The chip is 1GByte and has a 512K block size, and 4K pagesize with 224byte oob size.
If I run nand bad the whole flash chip is reported as bad.
Has anyone had a similar experiance? Any ideas what might be causing this?
Thanks for your help.
Code Changes to nand_ids.c
{"NAND 1GiB 3,3V 8-bit Custom", | 0x38, 0, 1024, 0, LP_OPTIONS} |
Code Changes nand_boot.c:
U-boot Output:
/* Check Micron device */ /* Check for 5 byte ID + Micron + read more 0x00 */ else if (id_data[0] == NAND_MFR_MICRON && id_data[4] != 0x00 && id_data[5] == 0x00 && id_data[6] == 0x00) {
/* Calc pagesize */ mtd->writesize = 1024 << (extid & 0x03); extid >>= 2;
/* OOB is 218B/224B per 4KiB pagesize */ mtd->oobsize = ((extid & 0x03) == 0x03 ? 218 : 224) << (mtd->writesize >> 13); extid >>= 3; /* Blocksize is multiple of 64KiB */ mtd->erasesize = mtd->writesize << (extid & 0x03) << 6; /* All Micron have busw x8? */ busw = 0;
printf("Micron id_data[0] = 0x%X, id_data[1] = 0x%X\n", id_data[0], id_data[1]); printf("Micron mtd->erasesize (block):%d\n", mtd->erasesize); printf("Micron mtd->writesize (page):%d\n", mtd->writesize); printf("Micron mtd->oobsize:%d\n", mtd->oobsize);
}
NAND boot...
U-Boot 2013.01-dirty (Nov 20 2013 - 15:55:35)
CPU: P1010, Version: 1.0, (0x80f10010)
Core: E500, Version: 5.1, (0x80212151)
Clock Configuration:
CPU0:800 MHz,
CCB:400 MHz,
DDR:333.333 MHz (666.667 MT/s data rate) (Asynchronous), IFC:100 MHz
L1: D-cache 32 kB enabled
I-cache 32 kB enabled
Board: P1010RDB
I2C: ready
SPI: ready
DRAM: Detected UDIMM Fixed DDR on board
1 GiB (DDR3, 32-bit, CL=5, ECC off)
Now running in RAM - U-Boot at: 3ff30000
L2: 256 KB enabled
NAND:
**** Additional Debug Information added ***
Micron id_data[0] = 0x2C, id_data[1] = 0x38
Micron mtd->erasesize (block):524288
Micron mtd->writesize (page):4096
Micron mtd->oobsize:224
1024 MiB
MMC: FSL_SDHC: 0
Bad block table not found for chip 0
Bad block table not found for chip 0
No space left to write bad block table
*** Warning - readenv() failed, using default environment
PCIe1: Root Complex of mini PCIe Slot, no link, regs @ 0xffe0a000
PCIe1: Bus 00 - 00
PCIe2: Root Complex of PCIe Slot, no link, regs @ 0xffe09000
PCIe2: Bus 01 - 01
In: serial
Out: serial
Err: serial
Net: PHY reset timed out
PHY reset timed out
eTSEC1 [PRIME], eTSEC2, eTSEC3
Hit any key to stop autoboot: 0
=> saveenv
Saving Environment to NAND...
Erasing Nand...
Skipping bad block at 0x00100000
Skipping bad block at 0x00180000
Skipping bad block at 0x00200000
Writing to Nand... FAILED!
=> nand info
Device 0: nand0, sector size 512 KiB
Page size 4096 b
OOB size 224 b
Erase size 524288 b
=>
解決済! 解決策の投稿を見る。
Please refer to the following Patch of P1010RDB-PB with MT29F16G08ABABAWP NAND.
/* old board P1010RDB uses 512M NAND */
/* new board P1010RDB-PB uses 4k-pagesize NAND 2GByte MT29F16G08ABABAWP NAND */
diff --git a/include/configs/P1010RDB.h b/include/configs/P1010RDB.h
index ba3f7c2..f2493c5 100644
--- a/include/configs/P1010RDB.h
+++ b/include/configs/P1010RDB.h
/*
* IFC Definitions
*/
@@ -322,6 +321,8 @@ extern unsigned long get_sdram_size(void);
| CSPR_MSEL_NAND \
| CSPR_V)
#define CONFIG_SYS_NAND_AMASK IFC_AMASK(64*1024)
+
+#if defined(CONFIG_P1010RDB)
#define CONFIG_SYS_NAND_CSOR (CSOR_NAND_ECC_ENC_EN /* ECC on encode */ \
| CSOR_NAND_ECC_DEC_EN /* ECC on decode */ \
| CSOR_NAND_ECC_MODE_4 /* 4-bit ECC */ \
@@ -329,13 +330,25 @@ extern unsigned long get_sdram_size(void);
| CSOR_NAND_PGS_512 /* Page Size = 512b */ \
| CSOR_NAND_SPRZ_16 /* Spare size = 16 */ \
| CSOR_NAND_PB(32)) /* 32 Pages Per Block */
+#define CONFIG_SYS_NAND_BLOCK_SIZE (16 * 1024)
+#elif defined(CONFIG_P1010RDB_PB)
+#define CONFIG_SYS_NAND_ONFI_DETECTION
+#define CONFIG_SYS_NAND_CSOR (CSOR_NAND_ECC_ENC_EN /* ECC on encode */ \
+ | CSOR_NAND_ECC_DEC_EN /* ECC on decode */ \
+ | CSOR_NAND_ECC_MODE_4 /* 4-bit ECC */ \
+ | CSOR_NAND_RAL_3 /* RAL = 3Byes */ \
+ | CSOR_NAND_PGS_4K /* Page Size = 4K */ \
+ | CSOR_NAND_SPRZ_224 /* Spare size = 224 */ \
+ | CSOR_NAND_PB(128)) /*Pages Per Block = 128 */
+#define CONFIG_SYS_NAND_BLOCK_SIZE (512 * 1024)
+#endif
#define CONFIG_SYS_NAND_BASE_LIST { CONFIG_SYS_NAND_BASE }
#define CONFIG_SYS_MAX_NAND_DEVICE 1
#define CONFIG_MTD_NAND_VERIFY_WRITE
#define CONFIG_CMD_NAND
-#define CONFIG_SYS_NAND_BLOCK_SIZE (16 * 1024)
+#if defined(CONFIG_P1010RDB)
/* NAND Flash Timing Params */
#define CONFIG_SYS_NAND_FTIM0 FTIM0_NAND_TCCST(0x01) | \
FTIM0_NAND_TWP(0x0C) | \
@@ -349,6 +362,22 @@ extern unsigned long get_sdram_size(void);
FTIM2_NAND_TREH(0x05) | \
FTIM2_NAND_TWHRE(0x0f)
#define CONFIG_SYS_NAND_FTIM3 FTIM3_NAND_TWW(0x04)
+#elif defined(CONFIG_P1010RDB_PB)
+/* support MT29F16G08ABABAWP 4k-pagesize 2G-bytes NAND */
+/* ONFI NAND Flash mode0 Timing Params */
+#define CONFIG_SYS_NAND_FTIM0 (FTIM0_NAND_TCCST(0x07)| \
+ FTIM0_NAND_TWP(0x18) | \
+ FTIM0_NAND_TWCHT(0x07) | \
+ FTIM0_NAND_TWH(0x0a))
+#define CONFIG_SYS_NAND_FTIM1 (FTIM1_NAND_TADLE(0x32)| \
+ FTIM1_NAND_TWBE(0x39) | \
+ FTIM1_NAND_TRR(0x0e) | \
+ FTIM1_NAND_TRP(0x18))
+#define CONFIG_SYS_NAND_FTIM2 (FTIM2_NAND_TRAD(0x0f) | \
+ FTIM2_NAND_TREH(0x0a) | \
+ FTIM2_NAND_TWHRE(0x1e))
+#define CONFIG_SYS_NAND_FTIM3 0x0
+#endif
#define CONFIG_SYS_NAND_DDR_LAW 11
#ifdef CONFIG_MMC
#define CONFIG_CMD_MMC
#define CONFIG_DOS_PARTITION
@@ -613,9 +647,14 @@ extern unsigned long get_sdram_size(void);
#define CONFIG_ENV_SIZE 0x2000
#elif defined(CONFIG_NAND)
#define CONFIG_ENV_IS_IN_NAND
+#if defined(CONFIG_P1010RDB)
#define CONFIG_ENV_SIZE CONFIG_SYS_NAND_BLOCK_SIZE
+#define CONFIG_ENV_RANGE (3 * CONFIG_ENV_SIZE) /* 3*16=48K for env */
+#elif defined(CONFIG_P1010RDB_PB)
+#define CONFIG_ENV_SIZE (16 * 1024)
+#define CONFIG_ENV_RANGE (32 * CONFIG_ENV_SIZE) /* new block size 512K */
+#endif
#define CONFIG_ENV_OFFSET ((512 * 1024) + CONFIG_SYS_NAND_BLOCK_SIZE)
-#define CONFIG_ENV_RANGE (3 * CONFIG_ENV_SIZE)
#elif defined(CONFIG_SYS_RAMBOOT)
#define CONFIG_ENV_IS_NOWHERE /* Store ENV in memory only */
#define CONFIG_ENV_ADDR (CONFIG_SYS_MONITOR_BASE - 0x1000)
I have a follow up question. NAND now fully works but on boot there is a message "fsl_ifc_read_buf beyond end of buffer (256 requested, 0 available)". This message originates from fsl_ifc_nand.c. Do you know what the cause of this message is?
Thanks again.
Uboot Output:
NAND boot...
U-Boot 2013.01-dirty (Nov 22 2013 - 16:30:00)
CPU: P1010, Version: 1.0, (0x80f10010)
Core: E500, Version: 5.1, (0x80212151)
Clock Configuration:
CPU0:800 MHz,
CCB:400 MHz,
DDR:333.333 MHz (666.667 MT/s data rate) (Asynchronous), IFC:100 MHz
L1: D-cache 32 kB enabled
I-cache 32 kB enabled
Board: P1010RDB
I2C: ready
SPI: ready
DRAM: Detected UDIMM Fixed DDR on board
1 GiB (DDR3, 32-bit, CL=5, ECC off)
Now running in RAM - U-Boot at: 3ff30000
L2: 256 KB enabled
NAND:
** ADDED Debug**
len = 256 ctrl->read_bytes = 256 ctrl->index = 256
ctrl->oob = 0 ctrl->eccread = 0
len = 256 ctrl->read_bytes = 256 ctrl->index = 256
ctrl->oob = 0 ctrl->eccread = 0
fsl_ifc_read_buf beyond end of buffer (256 requested, 0 available)
** ADDED Debug**
len = 256 ctrl->read_bytes = 256 ctrl->index = 256
ctrl->oob = 0 ctrl->eccread = 0
fsl_ifc_read_buf beyond end of buffer (256 requested, 0 available)
Micron id_data[0] = 0x2C, id_data[1] = 0x38
Micron mtd->erasesize (block):524288
Micron mtd->writesize (page):4096
Micron mtd->oobsize:224
Micron mtd->oobavail:0
1024 MiB
MMC: FSL_SDHC: 0
PCIe1: Root Complex of mini PCIe Slot, no link, regs @ 0xffe0a000
PCIe1: Bus 00 - 00
PCIe2: Root Complex of PCIe Slot, no link, regs @ 0xffe09000
PCIe2: Bus 01 - 01
In: serial
Out: serial
Err: serial
Net: PHY reset timed out
PHY reset timed out
eTSEC1 [PRIME], eTSEC2, eTSEC3
Hit any key to stop autoboot: 0
=>
Please refer to the following Patch of P1010RDB-PB with MT29F16G08ABABAWP NAND.
/* old board P1010RDB uses 512M NAND */
/* new board P1010RDB-PB uses 4k-pagesize NAND 2GByte MT29F16G08ABABAWP NAND */
diff --git a/include/configs/P1010RDB.h b/include/configs/P1010RDB.h
index ba3f7c2..f2493c5 100644
--- a/include/configs/P1010RDB.h
+++ b/include/configs/P1010RDB.h
/*
* IFC Definitions
*/
@@ -322,6 +321,8 @@ extern unsigned long get_sdram_size(void);
| CSPR_MSEL_NAND \
| CSPR_V)
#define CONFIG_SYS_NAND_AMASK IFC_AMASK(64*1024)
+
+#if defined(CONFIG_P1010RDB)
#define CONFIG_SYS_NAND_CSOR (CSOR_NAND_ECC_ENC_EN /* ECC on encode */ \
| CSOR_NAND_ECC_DEC_EN /* ECC on decode */ \
| CSOR_NAND_ECC_MODE_4 /* 4-bit ECC */ \
@@ -329,13 +330,25 @@ extern unsigned long get_sdram_size(void);
| CSOR_NAND_PGS_512 /* Page Size = 512b */ \
| CSOR_NAND_SPRZ_16 /* Spare size = 16 */ \
| CSOR_NAND_PB(32)) /* 32 Pages Per Block */
+#define CONFIG_SYS_NAND_BLOCK_SIZE (16 * 1024)
+#elif defined(CONFIG_P1010RDB_PB)
+#define CONFIG_SYS_NAND_ONFI_DETECTION
+#define CONFIG_SYS_NAND_CSOR (CSOR_NAND_ECC_ENC_EN /* ECC on encode */ \
+ | CSOR_NAND_ECC_DEC_EN /* ECC on decode */ \
+ | CSOR_NAND_ECC_MODE_4 /* 4-bit ECC */ \
+ | CSOR_NAND_RAL_3 /* RAL = 3Byes */ \
+ | CSOR_NAND_PGS_4K /* Page Size = 4K */ \
+ | CSOR_NAND_SPRZ_224 /* Spare size = 224 */ \
+ | CSOR_NAND_PB(128)) /*Pages Per Block = 128 */
+#define CONFIG_SYS_NAND_BLOCK_SIZE (512 * 1024)
+#endif
#define CONFIG_SYS_NAND_BASE_LIST { CONFIG_SYS_NAND_BASE }
#define CONFIG_SYS_MAX_NAND_DEVICE 1
#define CONFIG_MTD_NAND_VERIFY_WRITE
#define CONFIG_CMD_NAND
-#define CONFIG_SYS_NAND_BLOCK_SIZE (16 * 1024)
+#if defined(CONFIG_P1010RDB)
/* NAND Flash Timing Params */
#define CONFIG_SYS_NAND_FTIM0 FTIM0_NAND_TCCST(0x01) | \
FTIM0_NAND_TWP(0x0C) | \
@@ -349,6 +362,22 @@ extern unsigned long get_sdram_size(void);
FTIM2_NAND_TREH(0x05) | \
FTIM2_NAND_TWHRE(0x0f)
#define CONFIG_SYS_NAND_FTIM3 FTIM3_NAND_TWW(0x04)
+#elif defined(CONFIG_P1010RDB_PB)
+/* support MT29F16G08ABABAWP 4k-pagesize 2G-bytes NAND */
+/* ONFI NAND Flash mode0 Timing Params */
+#define CONFIG_SYS_NAND_FTIM0 (FTIM0_NAND_TCCST(0x07)| \
+ FTIM0_NAND_TWP(0x18) | \
+ FTIM0_NAND_TWCHT(0x07) | \
+ FTIM0_NAND_TWH(0x0a))
+#define CONFIG_SYS_NAND_FTIM1 (FTIM1_NAND_TADLE(0x32)| \
+ FTIM1_NAND_TWBE(0x39) | \
+ FTIM1_NAND_TRR(0x0e) | \
+ FTIM1_NAND_TRP(0x18))
+#define CONFIG_SYS_NAND_FTIM2 (FTIM2_NAND_TRAD(0x0f) | \
+ FTIM2_NAND_TREH(0x0a) | \
+ FTIM2_NAND_TWHRE(0x1e))
+#define CONFIG_SYS_NAND_FTIM3 0x0
+#endif
#define CONFIG_SYS_NAND_DDR_LAW 11
#ifdef CONFIG_MMC
#define CONFIG_CMD_MMC
#define CONFIG_DOS_PARTITION
@@ -613,9 +647,14 @@ extern unsigned long get_sdram_size(void);
#define CONFIG_ENV_SIZE 0x2000
#elif defined(CONFIG_NAND)
#define CONFIG_ENV_IS_IN_NAND
+#if defined(CONFIG_P1010RDB)
#define CONFIG_ENV_SIZE CONFIG_SYS_NAND_BLOCK_SIZE
+#define CONFIG_ENV_RANGE (3 * CONFIG_ENV_SIZE) /* 3*16=48K for env */
+#elif defined(CONFIG_P1010RDB_PB)
+#define CONFIG_ENV_SIZE (16 * 1024)
+#define CONFIG_ENV_RANGE (32 * CONFIG_ENV_SIZE) /* new block size 512K */
+#endif
#define CONFIG_ENV_OFFSET ((512 * 1024) + CONFIG_SYS_NAND_BLOCK_SIZE)
-#define CONFIG_ENV_RANGE (3 * CONFIG_ENV_SIZE)
#elif defined(CONFIG_SYS_RAMBOOT)
#define CONFIG_ENV_IS_NOWHERE /* Store ENV in memory only */
#define CONFIG_ENV_ADDR (CONFIG_SYS_MONITOR_BASE - 0x1000)
Thanks Yiping! :smileyhappy: That solved the issue.