P4080DS reflector is not working
Hi,
I am new to Freescale so my questions might be very basic
1. How to identify the revision of P4080DS board?
My u-boot prints "CPU0: P4080E, Version: 3.0" in the very startup, is this the revision?
2. as per the SDK fm1-gb1 port is used for Linux kernel which is on the main board, I am not able to ping through this port even the ifconfig shows it is RUNNING, port has RED led
contantly.
3. I do not have any XAUI card so I programmed SerDes 0x10 RCW rcw_5g_1500mhz.bin, uboot, fman to the flash and boot from bank4, I loaded fsl-image-core and trying sample
application reflector but it is giving following error
ERR : Invocation of FM_PORT_Open for fm1/port/1G/3 failed
ERR : Invocation of FM_PCD_Disable for fm0/pcd failed with error code 0x00010028
Found /fsl,dpaa/dpa-fman0-oh@1, Tx Channel = 46, FMAN = 0, Port ID = 1
Found /fsl,dpaa/ethernet@5, Tx Channel = 61, FMAN = 1, Port ID = 0
Found /fsl,dpaa/ethernet@6, Tx Channel = 62, FMAN = 1, Port ID = 1
Found /fsl,dpaa/ethernet@7, Tx Channel = 63, FMAN = 1, Port ID = 2
ERR: drivers/fman/fman.c:279:fman_if_init()
Unknown error -22: /soc@ffe000000/fman@500000/ethernet@e6000: no local-mac-address
ERR: drivers/fman/fman.c:449:fman_init()
Unknown error -22: if_init(/fsl,dpaa/ethernet@8)
Tearing down /fsl,dpaa/ethernet@5
Tearing down /fsl,dpaa/ethernet@6
Tearing down /fsl,dpaa/ethernet@7
apps/lib/usdpaa_netcfg_layer.c:488:usdpaa_netcfg_acquire(): fman driver init failed (ERRNO = -22)
error: failed to load configuration
I followed the steps given by the SDK. Any help is appreciated.
Regards,
Ankur.

The application reflector is a USDPAA based sample program, please make sure that you have boot up your system with a USDPAA dtb "uImage-p4080ds-usdpaa.dtb".
Before running USDPAA application, it is required to configure frame manger for the interfaces that will receive traffic. please use FMC commands on your target before start the reflector application. for example,
$ cd /usr/etc/
$ fmc –c usdpaa_config_p4_serdes_0x10.xml –p usdpaa_policy_hash_ipv4.xml –a.
If you want to use shared MAC between USDPAA and Linux, you could use the shared MAC dtb file p4080ds-usdpaa-shared-interfaces.dtb and shared MAC policy usdpaa_policy_hash_shared_mac_ipv4.xml.
About the Linux Kernel ping problem, please make sure fman ucode has been flashed correctly and MAC address has been configured correctly, please check whether this port can work in u-boot.
In application, please pay attention to the following configuration.
• SGMII card goes in P4080DS slot 3.
• Use SerDes 0x10 and RCW file: R_PPSXN_0x10/rcw_5g_1500mhz.bin in the
P4080DS NOR flash. This is a different RCW file than the one discussed above.
• Boot into bank 4 (assuming you are using bank 4 for USDPAA).
• Add text ";serdes:fsl_srds_lpd_b2=0xf" to u-boot environment variable hwconfig,
saveenv, and reset the system again into bank 4. This disables fm2-10g. The leading
";" separates the information added to hwconfig from what was already there. Note
that fm1-10g is never available in SerDes 0x10.
• Delete references to any of the 10 Gbps interfaces and ensure references to all
USDPAA 1 Gbps interfaces are present in the fmc configuration file. For example, it
should like the following after you edit it:
<cfgdata>
<config>
<engine name="fm1">
<port type="1G" number="0" policy="hash_ipv4_policy_5"/>
<port type="1G" number="1" policy="hash_ipv4_policy_6"/>
<port type="1G" number="2" policy="hash_ipv4_policy_7"/>
<port type="1G" number="3" policy="hash_ipv4_policy_8"/>
</engine>
</config>
</cfgdata>
Run the USDPAA application.
Thanks for your inputs, I will cross check on the dtb in use, for ping
issue some more questions
1. I am not able to ping using FM1@DTSEC2 port at all, I tried many times.
FMan was loaded, following is the boot log
2. I also do not have p4080ds-usdpaa-shared-interfaces.dtb file in image
directory, do we need to generate it by running some
special command.
U-Boot 2013.01 (Oct 21 2013 - 20:07:45)
CPU0: P4080E, Version: 3.0, (0x82080030)
Core: E500MC, Version: 3.1, (0x80230031)
Clock Configuration:
CPU0:1499.985 MHz, CPU1:1499.985 MHz, CPU2:1499.985 MHz,
CPU3:1499.985 MHz,
CPU4:1499.985 MHz, CPU5:1499.985 MHz, CPU6:1499.985 MHz,
CPU7:1499.985 MHz,
CCB:799.992 MHz,
DDR:649.994 MHz (1299.987 MT/s data rate) (Asynchronous), LBC:99.999
MHz
FMAN1: 599.994 MHz
FMAN2: 599.994 MHz
QMAN: 399.996 MHz
PME: 599.994 MHz
L1: D-cache 32 kB enabled
I-cache 32 kB enabled
Reset Configuration Word (RCW):
00000000: 105a0000 00000000 1e1e181e 0000cccc
00000010: 40464000 3c3c2000 de800000 e1000000
00000020: 00000000 00000000 00000000 008b6000
00000030: 00000000 00000000 00000000 00000000
Board: P4080DS, Sys ID: 0x17, Sys Ver: 0x01, FPGA Ver: 0x0c, vBank: 4
SERDES Reference Clocks: Bank1=100MHz Bank2=125MHz Bank3=125MHz
I2C: ready
SPI: ready
DRAM: Initializing....using SPD
Detected UDIMM i-DIMM
Detected UDIMM i-DIMM
2 GiB left unmapped
4 GiB (DDR3, 64-bit, CL=9, ECC off)
DDR Controller Interleaving Mode: cache line
DDR Chip-Select Interleaving Mode: CS0+CS1
Testing 0x00000000 - 0x7fffffff
Testing 0x80000000 - 0xffffffff
Remap DDR 2 GiB left unmapped
POST memory PASSED
Flash: 128 MiB
L2: 128 KB enabled
Corenet Platform Cache: 2048 KB enabled
SERDES: bank 2 disabled
SERDES: bank 3 disabled
SRIO1: disabled
SRIO2: disabled
MMC: FSL_SDHC: 0
EEPROM: NXID v1
PCIe1: Root Complex, no link, regs @ 0xfe200000
PCIe1: Bus 00 - 00
PCIe2: disabled
PCIe3: Root Complex, x1, regs @ 0xfe202000
02:00.0 - 1095:3132 - Mass storage controller
PCIe3: Bus 01 - 02
In: serial
Out: serial
Err: serial
Net: Fman1: Uploading microcode version 106.2.9
PHY reset timed out
Fman2: Uploading microcode version 106.2.9
FM1@DTSEC2, FM2@DTSEC1, FM2@DTSEC2, FM2@DTSEC3, FM2@DTSEC4
Hit any key to stop autoboot: 10 0
Thanks for your help.
Ankur.
On Fri, Nov 1, 2013 at 2:41 PM, Yiping Wang

Have you set these parameters in u-boot?
setenv ethact FM1@DTSEC2
setenv ethprime FM1@DTSEC2
Would you please share your u-boot environment variables and ping log?
In order to build p4080ds-usdpaa-shared-interfaces.dtb, please add "${S}/arch/powerpc/boot/dts/p4080ds-usdpaa-shared-interfaces.dts in variable KERNEL_DEVICETREE in meta-fsl-ppc/conf/machine/p4080ds.conf.
Then rebuild Kernel.

I have verified your u-boot environment on my target without any problem, please check whether there is physical connection problem on your target.
Thanks for you reply.
I am attaching logs from our board.
######################################################
U-Boot 2011.12-00064-gbfb0c9a (Jun 15 2012 - 16:09:09)
CPU0: P4080E, Version: 3.0, (0x82080030)
Core: E500MC, Version: 3.1, (0x80230031)
Clock Configuration:
CPU0:1499.985 MHz, CPU1:1499.985 MHz, CPU2:1499.985 MHz,
CPU3:1499.985 MHz,
CPU4:1499.985 MHz, CPU5:1499.985 MHz, CPU6:1499.985 MHz,
CPU7:1499.985 MHz,
CCB:799.992 MHz,
DDR:649.994 MHz (1299.987 MT/s data rate) (Asynchronous), LBC:99.999
MHz
FMAN1: 599.994 MHz
FMAN2: 599.994 MHz
PME: 399.996 MHz
L1: D-cache 32 kB enabled
I-cache 32 kB enabled
Board: P4080DS, Sys ID: 0x17, Sys Ver: 0x01, FPGA Ver: 0x0c, vBank: 0
36-bit Addressing
Reset Configuration Word (RCW):
00000000: 105a0000 00000000 1e1e181e 0000cccc
00000010: 40464000 3c3c2000 fe800000 61000000
00000020: 00000000 00000000 00000000 008b6000
00000030: 00000000 00000000 00000000 00000000
SERDES Reference Clocks: Bank1=100MHz Bank2=125MHz Bank3=125MHz
I2C: ready
SPI: ready
DRAM: Initializing....using SPD
Detected UDIMM i-DIMM
Detected UDIMM i-DIMM
CS2 is disabled.
CS3 is disabled.
CS2 is disabled.
CS3 is disabled.
2 GiB left unmapped
4 GiB (DDR3, 64-bit, CL=9, ECC off)
DDR Controller Interleaving Mode: cache line
DDR Chip-Select Interleaving Mode: CS0+CS1
Testing 0x00000000 - 0x7fffffff
Testing 0x80000000 - 0xffffffff
Remap DDR 2 GiB left unmapped
POST memory PASSED
Flash: 128 MiB
L2: 128 KB enabled
Corenet Platform Cache: 2048 KB enabled
SERDES: bank 2 disabled
SERDES: bank 3 disabled
SRIO1: disabled
SRIO2: disabled
MMC: FSL_SDHC: 0
EEPROM: NXID v1
PCIe1: Root Complex, no link, regs @ 0xfe200000
PCIe1: Bus 00 - 00
PCIe2: disabled
PCIe3: Root Complex, x1, regs @ 0xfe202000
02:00.0 - 1095:3132 - Mass storage controller
PCIe3: Bus 01 - 02
In: serial
Out: serial
Err: serial
Net: Fman1: Uploading microcode version 106.2.0
Fman2: Uploading microcode version 106.2.0
FM1@DTSEC2, FM2@DTSEC1, FM2@DTSEC2, FM2@DTSEC3, FM2@DTSEC4
Hit any key to stop autoboot: 5 4 3 2 1 0 ÿ
U-Boot 2013.01 (Oct 21 2013 - 20:07:45)
CPU0: P4080E, Version: 3.0, (0x82080030)
Core: E500MC, Version: 3.1, (0x80230031)
Clock Configuration:
CPU0:1499.985 MHz, CPU1:1499.985 MHz, CPU2:1499.985 MHz,
CPU3:1499.985 MHz,
CPU4:1499.985 MHz, CPU5:1499.985 MHz, CPU6:1499.985 MHz,
CPU7:1499.985 MHz,
CCB:799.992 MHz,
DDR:649.994 MHz (1299.987 MT/s data rate) (Asynchronous), LBC:99.999
MHz
FMAN1: 599.994 MHz
FMAN2: 599.994 MHz
QMAN: 399.996 MHz
PME: 599.994 MHz
L1: D-cache 32 kB enabled
I-cache 32 kB enabled
Reset Configuration Word (RCW):
00000000: 105a0000 00000000 1e1e181e 0000cccc
00000010: 40464000 3c3c2000 de800000 e1000000
00000020: 00000000 00000000 00000000 008b6000
00000030: 00000000 00000000 00000000 00000000
Board: P4080DS, Sys ID: 0x17, Sys Ver: 0x01, FPGA Ver: 0x0c, vBank: 4
SERDES Reference Clocks: Bank1=100MHz Bank2=125MHz Bank3=125MHz
I2C: ready
SPI: ready
DRAM: Initializing....using SPD
Detected UDIMM i-DIMM
Detected UDIMM i-DIMM
2 GiB left unmapped
4 GiB (DDR3, 64-bit, CL=9, ECC off)
DDR Controller Interleaving Mode: cache line
DDR Chip-Select Interleaving Mode: CS0+CS1
Testing 0x00000000 - 0x7fffffff
Testing 0x80000000 - 0xffffffff
Remap DDR 2 GiB left unmapped
POST memory PASSED
Flash: 128 MiB
L2: 128 KB enabled
Corenet Platform Cache: 2048 KB enabled
SERDES: bank 2 disabled
SERDES: bank 3 disabled
SRIO1: disabled
SRIO2: disabled
MMC: FSL_SDHC: 0
EEPROM: NXID v1
PCIe1: Root Complex, no link, regs @ 0xfe200000
PCIe1: Bus 00 - 00
PCIe2: disabled
PCIe3: Root Complex, x1, regs @ 0xfe202000
02:00.0 - 1095:3132 - Mass storage controller
PCIe3: Bus 01 - 02
In: serial
Out: serial
Err: serial
Net: Fman1: Uploading microcode version 106.2.9
PHY reset timed out
Fman2: Uploading microcode version 106.2.9
FM1@DTSEC2, FM2@DTSEC1, FM2@DTSEC2, FM2@DTSEC3, FM2@DTSEC4
Hit any key to stop autoboot: 10 0
=> printenv
baudrate=115200
bdev=sda3
bootargs=root=/dev/nfs rw nfsroot=172.16.124.136:/home/hitachi/tftpboot/yocto
ip=172.16.124.153:172.16.124.136::255.255.255.128::eth1:off
console=ttyS0,115200 usdpaa_mem=256M,1G
bootcmd=run cboot
bootdef=bootm 0xec020000 0xed300000 0xec800000
bootdelay=10
bootfile=uImage-p4080ds.bin
c=ffe
cboot=tftp 1000000 uImage-p4080ds.bin;tftp 0x2000000
fsl-image-core-p4080ds.ext2.gz.u-boot; tftp c00000
uImage-p4080ds-usdpaa.dtb;setenv bootargs usdpaa_mem=256M
usdpaa_mem=256M,1G;bootm 1000000 0x2000000 c00000
consoledev=ttyS0
eth1addr=00:04:9F:02:85:91
eth2addr=00:04:9F:02:85:92
eth3addr=00:04:9F:02:85:93
eth4addr=00:04:9F:02:85:94
eth5addr=00:04:9F:02:85:95
eth6addr=00:04:9F:02:85:96
eth7addr=00:04:9F:02:85:97
ethact=FM1@DTSEC2
ethaddr=00:04:9F:02:85:90
ethprime=FM1@DTSEC1
fdtaddr=c00000
fdtfile=uImage-p4080ds-usdpaa.dtb
fman_ucode=0xeff40000
gateway=172.16.124.129
hwconfig=serdes:fsl_srds_lpd_b2=0xf;fsl_ddr:ctlr_intlv=cacheline,bank_intlv=cs0_cs1,ecc=off
ipaddr=172.16.124.153
loadaddr=1000000
netdev=eth1
netmask=255.255.255.128
nfsboot=setenv bootargs root=/dev/nfs rw nfsroot=$serverip:$rootpath
ip=$ipaddr:$serverip:$gatewayip:$netmask:$hostname:$netdev:off
console=$consoledev,$baudrate $othbootargs;tftp $loadaddr $bootfile;tftp
$fdtaddr $fdtfile;bootm $loadaddr - $fdtaddr
othbootargs=bportals=s0-1 qportals=s0-1
ramboot=setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate
$othbootargs;tftp $ramdiskaddr $ramdiskfile;tftp $loadaddr $bootfile;tftp
$fdtaddr $fdtfile;bootm $loadaddr $ramdiskaddr $fdtaddr
ramdiskaddr=2000000
ramdiskfile=p4080ds/ramdisk.uboot
rfsaddr=0x2000000
rfsfile=fsl-image-core-p4080ds.ext2.gz.u-boot
rootpath=/home/hitachi/tftpboot/yocto
serverip=172.16.124.136
stderr=serial
stdin=serial
stdout=serial
tftpflash=tftpboot $loadaddr $uboot && protect off $ubootaddr +$filesize &&
erase $ubootaddr +$filesize && cp.b $loadaddr $ubootaddr $filesize &&
protect on $ubootaddr +$filesize && cmp.b $loadaddr $ubootaddr $filesize
uboot=u-boot.bin
ubootaddr=0xeff80000
Environment size: 2117/8188 bytes
=> run coo boot
Using FM1@DTSEC2 device
TFTP from server 172.16.124.136; our IP address is 172.16.124.153
Filename 'uImage-p4080ds.bin'.
Load address: 0x1000000
Loading: * T T T T T T T T T T
Retry count exceeded; starting again
Using FM2@DTSEC1 device
TFTP from server 172.16.124.136; our IP address is 172.16.124.153
Filename 'uImage-p4080ds.bin'.
Load address: 0x1000000
Loading: * #################################################################
#################################################################
#################################################################
#################################################################
##########
12.9 MiB/s
done
Bytes transferred = 3956560 (3c5f50 hex)
Using FM2@DTSEC1 device
TFTP from server 172.16.124.136; our IP address is 172.16.124.153
Filename 'fsl-image-core-p4080ds.ext2.gz.u-boot'.
Load address: 0x2000000
Loading: * #################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#######################################################
13 MiB/s
done
Bytes transferred = 27522881 (1a3f741 hex)
Using FM2@DTSEC1 device
TFTP from server 172.16.124.136; our IP address is 172.16.124.153
Filename 'uImage-p4080ds-usdpaa.dtb'.
Load address: 0xc00000
Loading: * ####
10.2 MiB/s
done
Bytes transferred = 53467 (d0db hex)
WARNING: adjusting available memory to 30000000
Booting kernel from Legacy Image at 01000000 ...
Image Name: Linux-3.8.13-rt9-QorIQ-SDK-V1.4
Image Type: PowerPC Linux Kernel Image (gzip compressed)
Data Size: 3956496 Bytes = 3.8 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
Loading init Ramdisk from Legacy Image at 02000000 ...
Image Name: fsl-image-core-p4080ds-201310240
Image Type: PowerPC Linux RAMDisk Image (gzip compressed)
Data Size: 27522817 Bytes = 26.2 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
Flattened Device Tree blob at 00c00000
Booting using the fdt blob at 0x00c00000
Uncompressing Kernel Image ... OK
Loading Ramdisk to 2e5c0000, end 2ffff701 ... OK
Loading Device Tree to 03fdf000, end 03fff0da ... OK
ERROR, usdpaa_mem arg is invalid
Using P4080 DS machine description
Memory CAM mapping: 256/256/256 Mb, residual: 3328Mb
Linux version 3.8.13-rt9-QorIQ-SDK-V1.4 (hitachi@HITTACHI-24) (gcc version
4.7.2 (GCC) ) #1 SMP Mon Oct 21 20:10:34 IST 2013
Found initrd at 0xee5c0000:0xeffff701
No /soc@ffe000000/qman@318000 property 'fsl,qman-fqd', using
memblock_alloc(0000000000400000)
No /soc@ffe000000/qman@318000 property 'fsl,qman-pfdr', using
memblock_alloc(0000000002000000)
Qman ver:0a01,01,02
No /soc@ffe000000/bman@31a000 property 'fsl,bman-fbpr', using
memblock_alloc(0000000001000000)
Bman ver:0a02,01,00
pme: No /soc@ffe000000/pme@316000 property 'fsl,pme-pdsr', using
memblock_alloc(0x0000000001000000)
pme: No /soc@ffe000000/pme@316000 property 'fsl,pme-sre', using
memblock_alloc(0x0000000000a00000)
USDPAA region at 10000000:10000000(10000:10000), 1 TLB1 entries)
CPU maps initialized for 1 thread per core
bootconsole enabled
setup_arch: bootmem
P4080 DS board from Freescale Semiconductor
arch: exit
Zone ranges:
DMA
Normal empty
HighMem
Movable zone start for each node
Early memory node ranges
node 0:
MMU: Allocated 1088 bytes of context maps for 255 contexts
PERCPU: Embedded 10 pages/cpu @c28d9000 s17216 r8192 d15552 u40960
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 1040384
Kernel command line: usdpaa_mem=256M usdpaa_mem=256M,1G
PID hash table entries: 4096 (order: 2, 16384 bytes)
Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
Memory: 3716020k/4194304k available (8116k kernel code, 478284k reserved,
304k data, 558k bss, 268k init)
Kernel virtual memory layout:
0xfff5f000..0xfffff000 : fixmap
0xffc00000..0xffe00000 : highmem PTEs
0xffbfa000..0xffc00000 : early ioremap
0xf1000000..0xffbfa000 : vmalloc & ioremap
Hierarchical RCU implementation.
RCU debugfs-based tracing is enabled.
NR_IRQS:512 nr_irqs:512 16
mpic: Setting up MPIC " OpenPIC " version 1.2 at ffe040000, max 8 CPUs
mpic: ISU size: 512, shift: 9, mask: 1ff
mpic: Initializing for 512 sources
clocksource: timebase mult[14000d1b] shift[24] registered
Console: colour dummy device 80x25
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 512
mpic: requesting IPIs...
e500 family performance monitor hardware support registered
Brought up 8 CPUs
devtmpfs: initialized
NET: Registered protocol family 16
Found FSL PCI host bridge at 0x0000000ffe200000. Firmware bus number: 0->0
PCI host bridge /pcie@ffe200000 (primary) ranges:
MEM 0x0000000c00000000..0x0000000c1fffffff -> 0x00000000e0000000
IO 0x0000000ff8000000..0x0000000ff800ffff -> 0x0000000000000000
/pcie@ffe200000: PCICSRBAR @ 0xdf000000
/pcie@ffe200000: Setup 64-bit PCI DMA window
/pcie@ffe200000: DMA window size is 0xdf000000
EDAC PCI0: Giving out device to module 'MPC85xx_edac' controller
'mpc85xx_pci_err': DEV 'ffe200000.pcie' (INTERRUPT)
MPC85xx_edac acquired irq 482 for PCI Err
MPC85xx_edac PCI err registered
Found FSL PCI host bridge at 0x0000000ffe202000. Firmware bus number: 0->1
PCI host bridge /pcie@ffe202000 ranges:
MEM 0x0000000c40000000..0x0000000c5fffffff -> 0x00000000e0000000
IO 0x0000000ff8020000..0x0000000ff802ffff -> 0x0000000000000000
/pcie@ffe202000: PCICSRBAR @ 0xdf000000
/pcie@ffe202000: Setup 64-bit PCI DMA window
/pcie@ffe202000: DMA window size is 0xdf000000
EDAC PCI1: Giving out device to module 'MPC85xx_edac' controller
'mpc85xx_pci_err': DEV 'ffe202000.pcie' (INTERRUPT)
MPC85xx_edac acquired irq 480 for PCI Err
MPC85xx_edac PCI err registered
software IO TLB (64MB) mapped at
PCI: Probing PCI hardware
fsl-pci ffe200000.pcie: PCI host bridge to bus 0000:00
pci_bus 0000:00: root bus resource
pci_bus 0000:00: root bus resource (bus
address )
pci_bus 0000:00: root bus resource
pci 0000:00:00.0: ignoring class 0x0b2000 (doesn't match header type 01)
pci 0000:00:00.0: bridge configuration invalid (), reconfiguring
pci 0000:00:00.0: PCI bridge to
fsl-pci ffe202000.pcie: PCI host bridge to bus 0001:02
pci_bus 0001:02: root bus resource (bus address
)
pci_bus 0001:02: root bus resource (bus
address )
pci_bus 0001:02: root bus resource
pci 0001:02:00.0: ignoring class 0x0b2000 (doesn't match header type 01)
PCIE error(s) detected
pci 0001:02:00.0: Primary bus is hard wired to 0
pci 0001:02:00.0: bridge configuration invalid (), reconfiguring
pci 0001:02:00.0: PCI bridge to
PCIE ERR_DR register: 0x80020000
PCIE ERR_CAP_STAT register: 0x80000001
PCIE ERR_CAP_R0 register: 0x00000800
PCIE ERR_CAP_R1 register: 0x00000000
PCIE ERR_CAP_R2 register: 0x00000000
PCIE ERR_CAP_R3 register: 0x00000000
pci 0000:00:00.0: PCI bridge to
pci 0000:00:00.0: bridge window
pci 0000:00:00.0: bridge window
pci 0001:02:00.0: BAR 9: can't assign mem pref (size 0x100000)
pci 0001:03:00.0: BAR 6: assigned
pci 0001:02:00.0: PCI bridge to
pci 0001:02:00.0: bridge window
pci 0001:02:00.0: bridge window
bio: create slab <bio-0> at 0
vgaarb: loaded
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
Bman err interrupt handler present
Bman portal initialised, cpu 0
Bman portal initialised, cpu 1
Bman portal initialised, cpu 2
Bman portal initialised, cpu 3
Bman portal initialised, cpu 4
Bman portal initialised, cpu 5
Bman portal initialised, cpu 6
Bman portal initialised, cpu 7
Bman portals initialised
Bman: BPID allocator includes range 32:32
Qman err interrupt handler present
Qman portal initialised, cpu 0
Qman portal initialised, cpu 1
Qman portal initialised, cpu 2
Qman portal initialised, cpu 3
Qman portal initialised, cpu 4
Qman portal initialised, cpu 5
Qman portal initialised, cpu 6
Qman portal initialised, cpu 7
Qman portals initialised
Qman: FQID allocator includes range 256:256
Qman: FQID allocator includes range 32768:32768
Qman: CGRID allocator includes range 0:256
Qman: pool channel allocator includes range 33:15
Switching to clocksource timebase
NET: Registered protocol family 2
TCP established hash table entries: 8192 (order: 4, 65536 bytes)
TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
TCP: Hash tables configured (established 8192 bind 8192)
TCP: reno registered
UDP hash table entries: 512 (order: 2, 16384 bytes)
UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
rootfs image is not initramfs (no cpio magic); looks like an initrd
Freeing initrd memory: 26880k freed
fsl-rcpm ffe0e2000.global-utilities: Freescale RCPM driver
audit: initializing netlink socket (disabled)
type=2000 audit(0.492:1): initialized
bounce pool size: 64 pages
HugeTLB registered 1 MB page size, pre-allocated 0 pages
HugeTLB registered 4 MB page size, pre-allocated 0 pages
HugeTLB registered 16 MB page size, pre-allocated 0 pages
HugeTLB registered 64 MB page size, pre-allocated 0 pages
HugeTLB registered 256 MB page size, pre-allocated 0 pages
HugeTLB registered 1 GB page size, pre-allocated 0 pages
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
NTFS driver 2.1.30 .
jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
msgmni has been set to 654
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
serial8250.0: ttyS0 at MMIO 0xffe11c500 (irq = 36) is a 16550A
console enabled, bootconsole disabled
console enabled, bootconsole disabled
serial8250.0: ttyS1 at MMIO 0xffe11c600 (irq = 36) is a 16550A
serial8250.0: ttyS2 at MMIO 0xffe11d500 (irq = 37) is a 16550A
serial8250.0: ttyS3 at MMIO 0xffe11d600 (irq = 37) is a 16550A
ePAPR hypervisor byte channel driver
Generic non-volatile memory driver v1.1
brd: module loaded
loop: module loaded
st: Version 20101219, fixed bufsize 32768, s/g segs 256
scsi0 : sata_sil24
scsi1 : sata_sil24
ata1: SATA max UDMA/100 host m128@0xc40000000 port 0xc40004000 irq 42
ata2: SATA max UDMA/100 host m128@0xc40000000 port 0xc40006000 irq 42
fe8000000.flash: Found 1 x16 devices at 0x0 in 16-bit bank. Manufacturer ID
0x000001 Chip ID 0x002801
Amd/Fujitsu Extended Query Table at 0x0040
Amd/Fujitsu Extended Query version 1.3.
number of CFI chips: 1
fsl_espi ffe110000.spi: master is unqueued, this is deprecated
m25p80 spi32766.0: s25sl12801 (16384 Kbytes)
4 ofpart partitions found on MTD device spi32766.0
Creating 4 MTD partitions on "spi32766.0":
0x000000000000-0x000000100000 : "u-boot"
0x000000100000-0x000000600000 : "kernel"
0x000000600000-0x000000700000 : "dtb"
0x000000700000-0x000001000000 : "file system"
fsl_espi ffe110000.spi: at 0xf117c000 (irq = 53)
libphy: Fixed MDIO Bus: probed
platform mdio-mux-emi1.14: Driver mdio-mux-gpio requests probe deferral
platform mdio-mux-emi2.15: Driver mdio-mux-gpio requests probe deferral
libphy: Freescale PowerQUICC MII Bus: probed
libphy: Freescale XGMAC MDIO Bus: probed
FMAN(0) Fifo size settings:
- Total buffers available(512 - 256B/buffer)
- Total throughput(1Gbps)
- Max frame size(1522B)
- 1G ports TX 1(12 bufs set (min: 12))
- 1G ports RX 1(452 bufs set (min: 14))
- OH-HC ports 4(8)
- Shared extra buffers(16)
FMAN(0) open dma settings:
- Total open dma available(32)
- 1G ports TX 1(14)
- 1G ports RX 1(14)
- OH-HC ports 4(1)
- Shared extra open dma(0)
FMAN(0) Tnums settings:
- Total Tnums available(128)
- 1G ports TX 1(59)
- 1G ports RX 1(59)
- OH-HC ports 4(2)
- Shared extra tnums(2)
FMAN(1) Fifo size settings:
- Total buffers available(512 - 256B/buffer)
- Total throughput(4Gbps)
- Max frame size(1522B)
- 1G ports TX 4(12 bufs set (min: 12))
- 1G ports RX 4(104 bufs set (min: 14))
- OH-HC ports 4(8)
- Shared extra buffers(16)
FMAN(1) open dma settings:
- Total open dma available(32)
- 1G ports TX 4(4)
- 1G ports RX 4(3)
- OH-HC ports 4(1)
- Shared extra open dma(0)
FMAN(1) Tnums settings:
- Total Tnums available(128)
- 1G ports TX 4(14)
- 1G ports RX 4(15)
- OH-HC ports 4(2)
- Shared extra tnums(4)
Freescale FM module (Oct 21 2013:20:09:58), FMD API version 21.1.0
Freescale FM Ports module (Oct 21 2013:20:09:57)
dpaa_debugfs: FSL DPAA Ethernet debugfs entries ()
fsl_mac: mac.c:417:mac_load() fsl_mac: FSL FMan MAC API based driver ()
fsl_mac ffe4e0000.ethernet: FMan dTSEC version: 0x08240101
fsl_mac ffe4e0000.ethernet: FMan MAC address: 00:04:9f:02:85:90
fsl_mac ffe4e2000.ethernet: FMan dTSEC version: 0x08240101
fsl_mac ffe4e2000.ethernet: FMan MAC address: 00:04:9f:02:85:91
fsl_mac ffe5e0000.ethernet: FMan dTSEC version: 0x08240101
fsl_mac ffe5e0000.ethernet: FMan MAC address: 00:04:9f:02:85:95
fsl_mac ffe5e2000.ethernet: FMan dTSEC version: 0x08240101
fsl_mac ffe5e2000.ethernet: FMan MAC address: 00:04:9f:02:85:96
fsl_mac ffe5e4000.ethernet: FMan dTSEC version: 0x08240101
fsl_mac ffe5e4000.ethernet: FMan MAC address: 00:04:9f:02:85:97
fsl_mac ffe5e6000.ethernet: of_get_mac_address(/soc@ffe000000/fman@500000
/ethernet@e6000) failed
fsl_mac: probe of ffe5e6000.ethernet failed with error -22
fsl_dpa: dpaa_eth.c:4320:dpa_load() fsl_dpa: FSL DPAA Ethernet driver ()
fsl_dpa ethernet.17: Using private BM buffer pools
fsl_dpa: dpaa_eth.c:3715:dpa_rx_fq_init() Using dynamic RX QM frame queues
fsl_dpa: dpaa_eth.c:3739:dpa_tx_fq_init() Using dynamic TX QM frame queues
fsl_dpa ethernet.21: dev_get_drvdata(ffe5e6000.ethernet) failed
fsl_dpa: probe of ethernet.21 failed with error -22
fsl_oh: offline_port.c:439:oh_port_load() fsl_oh: FSL FMan Offline Parsing
port driver ()
fsl_oh dpa-fman0-oh.22: Found OH node handle compatible with fsl,dpa-oh.
fsl_oh dpa-fman0-oh.22: OH port /soc@ffe000000/fman@400000/port@82000 has
no buffer pool. Fragmentation will not be enabled
fsl_oh dpa-fman0-oh.22: OH port /soc@ffe000000/fman@400000/port@82000enabled.
e1000: Intel(R) PRO/1000 Network Driver - version 7.3.21-k8-NAPI
e1000: Copyright (c) 1999-2006 Intel Corporation.
e1000e: Intel(R) PRO/1000 Network Driver - 2.1.4-k
e1000e: Copyright(c) 1999 - 2012 Intel Corporation.
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-pci: EHCI PCI platform driver
ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
/soc@ffe000000/usb@210000: Invalid 'dr_mode' property, fallback to host mode
fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller
fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1
fsl-ehci fsl-ehci.0: irq 44, io mem 0xffe210000
fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
Initializing USB Mass Storage driver...
usbcore: registered new interface driver usb-storage
USB Mass Storage support registered.
i2c /dev entries driver
mpc-i2c ffe118100.i2c: timeout 1000000 us
rtc-ds3232 0-0068: rtc core: registered ds3232 as rtc0
mpc-i2c ffe118000.i2c: timeout 1000000 us
mpc-i2c ffe119000.i2c: timeout 1000000 us
mpc-i2c ffe119100.i2c: timeout 1000000 us
EDAC MC: Ver: 3.0.0
Freescale(R) MPC85xx EDAC driver, (C) 2006 Montavista Software
mpc85xx_mc_err_probe: No ECC DIMMs discovered
mpc85xx_mc_err_probe: No ECC DIMMs discovered
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
mmc0: SDHCI controller on ffe114000.sdhc using DMA
platform caam_qi.0: Linux CAAM Queue I/F driver initialised
caam ffe300000.crypto: device ID = 0x0a10030000000000 (Era -524)
caam ffe300000.crypto: job rings = 4, qi = 1
caam ffe300000.crypto: fsl,sec-v4.0 algorithms registered in /proc/crypto
platform ffe301000.jr: registering rng-caam
platform caam_qi.0: fsl,sec-v4.0 algorithms registered in /proc/crypto
Freescale USDPAA process driver
Freescale USDPAA process IRQ driver
fsl-pme ffe316000.pme: ver: 0x00100201
Freescale pme2 db driver
Freescale pme2 scan driver
fsl-pme2-scan: device pme_scan registered
Freescale hypervisor management driver
fsl-hv: no hypervisor found
IPv4 over IPv4 tunneling driver
TCP: cubic registered
Initializing XFRM netlink socket
NET: Registered protocol family 10
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
NET: Registered protocol family 15
Key type dns_resolver registered
libphy: mdio_mux: probed
libphy: mdio_mux: probed
mdio-mux-gpio mdio-mux-emi1.14: Version 1.0
rtc-ds3232 0-0068: setting system clock to 2013-10-28 03:50:22 UTC
(1382932222)
ata1: SATA link up 3.0 Gbps (SStatus 123 SControl 0)
ata1.00: ATA-8: Hitachi HDS721050CLA360, JP2OA50E, max UDMA/133
ata1.00: 976773168 sectors, multi 0: LBA48 NCQ (depth 31/32)
ata1.00: configured for UDMA/100
scsi 0:0:0:0: Direct-Access ATA Hitachi HDS72105 JP2O PQ: 0 ANSI: 5
sd 0:0:0:0: 976773168 512-byte logical blocks: (500 GB/465 GiB)
sd 0:0:0:0: Attached scsi generic sg0 type 0
sd 0:0:0:0: Write Protect is off
sd 0:0:0:0: Write cache: enabled, read cache: enabled, doesn't
support DPO or FUA
sda: unknown partition table
sd 0:0:0:0: Attached SCSI disk
ata2: SATA link down (SStatus 0 SControl 0)
RAMDISK: gzip image found at block 0
VFS: Mounted root (ext2 filesystem) readonly on device 1:0.
devtmpfs: mounted
Freeing unused kernel memory: 268k freed
INIT: version 2.88 booting
/etc/init.d/rcS: line 27: /etc/hostname: Read-only file system
Starting udev
udevd[966]: starting version 182
Starting Bootlog daemon: bootlogd: cannot allocate pseudo tty: No such file
or directory
bootlogd.
Configuring network interfaces... done.
net.ipv4.conf.default.rp_filter = 0
net.ipv4.conf.all.rp_filter = 0
Running postinst /etc/rpm-postinsts/debianutils...
Running postinst /etc/rpm-postinsts/sysvinit-inittab...
INIT: Entering runlevel: 5
Starting Dropbear SSH server: Will output 1024 bit rsa secret key to
'/etc/dropbear/dropbear_rsa_host_key'
Generating key, this may take a while...
Public key portion is:
ssh-rsa
AAAAB3NzaC1yc2EAAAADAQABAAAAgwCi7BQQH2u2JvfBYUA10hWaN8A9b4NCIr/gkRNQewAGInOQGjgoGR96psWLrsXsOVcwFxfeDvBStM8IcevAi3lbE8v9raDfa/8ZCTWUiEmvL5ny5KU0kglqxW4lMe13k+uvjXR7cTiMfLvg7GpfA429miaByjAyDdhGZod2/jIGRp
root@p4080ds
Fingerprint: md5 dc:f5:02:08:8d:35:5e:24:2e:b3:ab:de:6a:c4:bb:b6
dropbear.
Starting network benchmark server: netserver.
Starting system log daemon...0
Starting kernel log daemon...0
Stopping Bootlog daemon: bootlogd.
Poky 9.0 (Yocto Project 1.4 Reference Distro) 1.4 p4080ds ttyS0
p4080ds login: 0xebf40000 root
root@p4080ds:~#
root@p4080ds:~#
root@p4080ds:~# cat /root/ ifcon fig
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
root@p4080ds:~# ifconfig -a
fm1-gb1 Link encap:Ethernet HWaddr 00:04:9f:02:85:91
BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Memory:fe4e2000-fe4e2fff
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
sit0 Link encap:UNSPEC HWaddr
00-00-00-00-00-00-10-0D-00-00-00-00-00-00-00-00
NOARP MTU:1480 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
tunl0 Link encap:IPIP Tunnel HWaddr
NOARP MTU:1480 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
######################################################
Regards,
Ankur.
On Mon, Nov 4, 2013 at 2:07 PM, Yiping Wang