P2041 is able to go for thermal shutdown or not

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

P2041 is able to go for thermal shutdown or not

592 Views
avinashh
Contributor III

HI,

we are using P2041 in conduction cooled systems. I want to know whether P2041 is able to go for thermal shutdown when it reaches maximum Junction temperature.
Also I want to control this using software at certain temperature say 100 dec C and also want to put the processor in sleep mode whenever required.

Can anyone suggest  whether these things are possible or not?

--regards,
Avinash

Labels (1)
0 Kudos
3 Replies

367 Views
avinashh
Contributor III

Thanks for the reply Alexander.

I have already kept sensor externally to sense junction temp of processor.

With this junction temperature readings, can I control following things:

a. Automatic shutdown is it available by default or with SW I have to do?

b. Change in temp threshold for shutdown through SW?

--regards,

Avinash

0 Kudos

367 Views
alexander_yakov
NXP Employee
NXP Employee

As I already said, this function should be implemented in user software.

Please address these questions to your software vendor.

0 Kudos

367 Views
alexander_yakov
NXP Employee
NXP Employee

This function should be implemented in user software, using external temperature detection circuitry.

Please look P2040 Reference Manual, Section 1.9.3 for details


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos