MDIC0 and MDIC1 resistor power for P2020

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MDIC0 and MDIC1 resistor power for P2020

1,645 次查看
toddreed
Contributor I

Hello,

I need to ensure that the MDIC resistors do not fail derated power limits.  What is the estimated power usage for a 40.2 ohm resistor on MDIC0 and MDIC1?

Thank you,

Todd

 

标签 (1)
0 项奖励
3 回复数

1,638 次查看
toddreed
Contributor I

Hi Bulat,

Thank you for your response.  I currently have 0603 resistors in there that are rated for 0.1W max, but I have to derate them to 0.056W.  Is this OK, or should my derated max be > 0.1W?

Thanks,

Todd

 

0 项奖励

1,618 次查看
Bulat
NXP Employee
NXP Employee

Yes, it is OK. 'Maximum theoretical power' can be calculated as GVDD x GVDD / 40.2. This results in about 80mW for DDR2 and 56mW for DDR3. In fact the peak power dissipation would be less, so no problem with resistor's size.

Regards,

Bulat

 

0 项奖励

1,639 次查看
Bulat
NXP Employee
NXP Employee

Those resistors are used during hw calibrations, i.e. relatively short time. Theoretically possible peak power is less than 0.1W, so resistors size 0402 is ok.

Regards,

Bulat

 

0 项奖励