P1020/P1011 SPI Specific FAQs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P1020/P1011 SPI Specific FAQs

P1020/P1011 SPI Specific FAQs

If SPI is not being used, how should SPI_CLK and SPI_MOSI be terminated in P1020/P1011?

SPI_CLK and SPI_MOSI should be pulled up, if not used.


ラベル(1)
コメント

According to P1020 Design Checklist (AN4259), SPI_CLK should be pulled down with 1K to GND if not used. Can anyone confirm which is the correct way?

Also confused on this...

See comment from AP application team:

Both are correct and expecting both of them works fine. The general idea of terminating unused signal is to set it to inactive state.


評価なし
バージョン履歴
最終更新日:
‎07-25-2012 10:39 AM
更新者: