does sja1110 supports whitelist

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

does sja1110 supports whitelist

Jump to solution
340 Views
ericpeng
Contributor I

HI, everyone. i'm choosing one switch and met with two issues with SJA1110 , and i did not get a certain answer in the datasheet

And trying to find a help here. Thanks you all, first. 

1. About whitelist. If i can control the flows only with some specific SMAC to be forwarded, while other SMACs dropped ? 

2. how flows are treated, dropped or forwarded , when they are not matchable with any rules set in DPI ?

0 Kudos
Reply
1 Solution
292 Views
kaden
NXP Employee
NXP Employee

Hi @ericpeng 

1. SJA1110 does support the concept of allowlists for SAs. If you have access to the documentation, please refer to the software application notes AN12925, chapter "6.6 MAC address allowlist". 

2. If there is no entry in the DPI, the flow will be handled according to the L2 Lookup/ L2 Policing and L2 Forwarding tables. DPI Table is not a mandatory table for the switch to be able to do L2 bridging. 

BR

Kaden

View solution in original post

1 Reply
293 Views
kaden
NXP Employee
NXP Employee

Hi @ericpeng 

1. SJA1110 does support the concept of allowlists for SAs. If you have access to the documentation, please refer to the software application notes AN12925, chapter "6.6 MAC address allowlist". 

2. If there is no entry in the DPI, the flow will be handled according to the L2 Lookup/ L2 Policing and L2 Forwarding tables. DPI Table is not a mandatory table for the switch to be able to do L2 bridging. 

BR

Kaden