codewarrior V8.8 MPC8640 JTAG接口需要使用什么型号的下载器?CWH-CTP-BASE-HE这个支持8640么?有没有官方的DDR控制程序(demo)可以用?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

codewarrior V8.8 MPC8640 JTAG接口需要使用什么型号的下载器?CWH-CTP-BASE-HE这个支持8640么?有没有官方的DDR控制程序(demo)可以用?

531 Views
HILL8195
Contributor I

由于实验需要,需要在MPC8640上运行DDR测试程序,来验证DDR2的功能。

在论坛上确认只能使用CW 8.8  版本,下载器目前还未购买,CWH-CTP-BASE-HE和CWH-UTP-PPCC-HE这两个下载器哪款可以支持MPC8640   JTAG接口?

是否有DDR测试 DEMO或程序可以参考?

0 Kudos
3 Replies

515 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please purchase CWH-CTP-BASE-HE

You could create a bareboard project in CodeWarrior IDE from File->New->EPPC New Project Wizard->Freescale PowerPC EABI Linker for MPC8641HPCN, then modify DDR2 initialization section in CodeWarrior initialization file PowerPC_EABI_Support\Initialization_Files\Host\8641DHPCN_init_core0.cfg according to your custom board, then click "debug" icon to initialize the target board and download the sample program to DDR and debug it in DDR.

0 Kudos

507 Views
HILL8195
Contributor I

HI yipingwang,

关于CW8.8的应用网上资源较少,可以提供相关使用指南或相关教程么?

0 Kudos

461 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the user guide in C:\Program Files (x86)\Freescale\CodeWarrior PA V8.8\Help\PDF\Pro & Linux App Edition Targeting Manual.pdf

0 Kudos