boot issue with LS1028ARDB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

boot issue with LS1028ARDB

551 次查看
cm1
Contributor I

Hi everyone,

I used nxp_LS1028ardb. And I did SDcardboot up with ubuntu 20.04 while following Open Industrial User Guide rev1.10(12/2020).

When I start the board, some "failed" commands come up.(the log is attached)

Should I need to install anything additionally after SDcardboot? what I have to do to resolve the errors?

Thanks for your help.

cm1_5-1632832644795.png

cm1_1-1632832504881.pngcm1_2-1632832528051.png

cm1_3-1632832587816.pngcm1_4-1632832615408.png

 

0 项奖励
1 回复

525 次查看
ufedor
NXP Employee
NXP Employee
0 项奖励