Using PTN5150 in DFM only what then about VBUS_DET?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using PTN5150 in DFM only what then about VBUS_DET?

Jump to solution
1,114 Views
thomaskofoedhan
Contributor III

I want to use the PTN5150 for a DFM application only with 3A capability, but what should I do with the VBUS_DET pin?

Thomas

Tags (2)
1 Solution
979 Views
thomaskofoedhan
Contributor III

Thank you Jose, for the answer. Clear and precise 

View solution in original post

0 Kudos
2 Replies
979 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

When the PTN5110 controller is configured as a DFP mode application only, the VBUS_DET pin can be left unconnected.

Regards,

Jose

980 Views
thomaskofoedhan
Contributor III

Thank you Jose, for the answer. Clear and precise 

0 Kudos