T2080 SerDes1_LNnGCR0 PROTS field

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T2080 SerDes1_LNnGCR0 PROTS field

528件の閲覧回数
scottgerhold
Contributor IV

In the T2080 Ref Manual, Rev 4, 04/2021 the PROTS field (bits 20:24) in SerDesx_LNnGCR0 in section 19.4.18 is defined for some options but not all. We have SRDS_PRTCL_S1 in the RCW set to 0x66, so lane 3 (D) is configured for XFI. The SerDes1_LN3GCR0[PROTS] field is reporting 01010 which isn't defined in the Reference Manual. But the reference manual doesn't define what XFI should report in the  PROTS field. Please let us know what the value should be when the lane is configured for XFI.

0 件の賞賛
返信
1 返信

511件の閲覧回数
Oswalag
NXP TechSupport
NXP TechSupport

The value "01010'' for SerDes1_LN3GCR0[PROTS] is correct for XFI 10GBase-KR

Regards,

Oswaldo.

0 件の賞賛
返信