Spice Model Files For BFU768F

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Spice Model Files For BFU768F

跳至解决方案
1,768 次查看
derekdszymanski
Contributor I

I'm looking for access to Spice files for BFU768F. Is this something the company will provide? If not, which Spice model should be used to calculate the correct characteristics for this part using the datasheet entries? Are there any other tools that can be used to extract the values for the model?

0 项奖励
回复
1 解答
1,708 次查看
LPP
NXP Employee
NXP Employee

BFU768F is a variance of BFU760F (selection optimized to operate at 10.8mA). You can use models for BFU760F to simulate BFU768F design.

BFU760F SPICE and MEXTRAM models are provided as a parts of NXP RF small signal kit for Keysight ADS tool.
https://www.nxp.com/products/rf/rf-discrete-components-low-power/rf-wideband-transistors/6-18-ghz-wi...

Also, you can find BFU760F S-parameters on it's web page:
https://www.nxp.com/products/rf/rf-discrete-components-low-power/rf-wideband-transistors/6-18-ghz-wi...

Note, BFU760F SPICE model is available on NXP site: https://www.nxp.com/downloads/en/spice-model/BFU760F.prm
Unfortunately, the quality of the SPICE model is poor and it doesn't match measured RF performance.

My suggestion for you is to use BFU760F SPICE model for DC simulation and S-parameters for RF design.

Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,708 次查看
derekdszymanski
Contributor I

Thank you for your help.

0 项奖励
回复
1,709 次查看
LPP
NXP Employee
NXP Employee

BFU768F is a variance of BFU760F (selection optimized to operate at 10.8mA). You can use models for BFU760F to simulate BFU768F design.

BFU760F SPICE and MEXTRAM models are provided as a parts of NXP RF small signal kit for Keysight ADS tool.
https://www.nxp.com/products/rf/rf-discrete-components-low-power/rf-wideband-transistors/6-18-ghz-wi...

Also, you can find BFU760F S-parameters on it's web page:
https://www.nxp.com/products/rf/rf-discrete-components-low-power/rf-wideband-transistors/6-18-ghz-wi...

Note, BFU760F SPICE model is available on NXP site: https://www.nxp.com/downloads/en/spice-model/BFU760F.prm
Unfortunately, the quality of the SPICE model is poor and it doesn't match measured RF performance.

My suggestion for you is to use BFU760F SPICE model for DC simulation and S-parameters for RF design.

Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复