Hello:
Are there any risk to short the SPI input and the RX_DV of port0 ? I have a mistake of HW design so I have to short the two pins.
I have tried once but the transmission of other ports does not work. So I break the connection.
By the way , can we config the SJA1105Q via Jtag interface? Then I will not need to take a risk to short two pins above.
Thanks!
Unfortunately you can't short SPI port to others pin and Jtag can't be used in SJA1105 which is not the MCU or processor.