SJA1105 power suppply

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SJA1105 power suppply

Jump to solution
256 Views
haiyang
Contributor III

hi,

i use the sja1105 to designed a ethernet switch.

i reference the SJA1105UM and MPC-LS-VNP-RDB board (SCH-45700).
int the SJA1105UM refer to:

haiyang_0-1703640945001.png

so,i think the VDDIO_MIIX  pin only can be supply 2.5V or 3.3V .

But in the MPC-LS-VNP-RDB board (SCH-45700), it show :

haiyang_2-1703641101515.png

the VDDIO_MII4  supply 1.2V.

so , whether have some err in the different doc?

haiyang

best wish. 

 

 

 

Tags (1)
0 Kudos
1 Solution
242 Views
guoweisun
NXP TechSupport
NXP TechSupport

The SGMII port on SJA1105R/S has two supply domains: 1.2V and 2.5V for analog IO.

View solution in original post

0 Kudos
1 Reply
243 Views
guoweisun
NXP TechSupport
NXP TechSupport

The SGMII port on SJA1105R/S has two supply domains: 1.2V and 2.5V for analog IO.

0 Kudos