SC18IM704-EVB, Is it OK to leave GPIO4 and 5 open?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SC18IM704-EVB, Is it OK to leave GPIO4 and 5 open?

259 次查看
Yuji_M2
Contributor I

On the circuit diagram, it is directly connected to the pin header in a floating state, but when the power is turned on, it should be an input setting, so an undefined value is read.
Is there a risk of destroying the IC due to shoot-through current when reading an undefined value?
Since there is a Schmidt trigger buffer, can I assume that there is no problem with input only?

0 项奖励
回复
0 回复数