I am debugging an new S32evb, and set the jumper according to the userguide,use "Win32 Disk Imager" to write "fsl-image-auto-s32evb.sdcard" directly to SD card,Insert the SDcard in the evb and start the board,My PuTTY printed the following information:
NOTICE: Reset status: Power-On Reset
NOTICE: BL2: v2.5(release):bsp33.0_rc9-2.5-dirty
NOTICE: BL2: Built : 14:01:09, Jun 15 2022
ERROR: No memory node found
ERROR: BL2: Failure in post image load handling (-11)
please help , thanks in advance :))
已解决! 转到解答。
Hello,
You have burn wrong the sdcard, try again:
https://www.nxp.com/docs/en/quick-reference-guide/S32G-VNP-EVB-QSG.pdf
Regards
Hello,
You have burn wrong the sdcard, try again:
https://www.nxp.com/docs/en/quick-reference-guide/S32G-VNP-EVB-QSG.pdf
Regards
Thanks for your reply, there is another problem: EVB can be started from SDcard, and oal_driver. ko needs to be loaded when running example. Execute modprobe oal_driver.ko according to the instructions of User Manual, and an error is reported:
Modprobe :FATAL:Module oal_driver.ko not found in driectory /lib/modeles/5.10.109-rt65+ g0Bace7fde5f5, run depmod Oal_driver. ko and another error is reported:
DEPMOD: ERROR: Bad version passed oal_driver.ko.
How do I resolve the problem?