BSP34.0 roofts,image
refer : S32R45_RSDK__1.0.0/Docs/RSDK_User_Manual.
the RSDK Linux kernel modules (*.ko) are now part of the boot image (in /lib/modules/'uname -r'/extra folder
but modprobe oal_driver ,SPT_driver fail,there is no oal_driver in /lib/modules/'uname -r'/extra folder? where I can find the right version SPT_driver ,oal_driverwith BSP34.0 ?
PS C:\NXP\S32R45_RSDK__1.0.0\SPT\SPT_driver\build\linux_kernel\rsdk_spt_driver is not fit with BSP34.0
Hello,
SImple solution is to use RSDK 1.1.0. The 1.0.0 release works with BSP 3.3.0 as stated in the release notes.
best regards,
Peter
Hello,
I have asked our RADAR team to have a look at your issue.
Best regards,
Peter