RDDRONE-T1ADAPT works only when connected to slave

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RDDRONE-T1ADAPT works only when connected to slave

84 Views
wlan
Contributor II

Hello,

We're using the RDDRONE-T1ADAPT to connect a board in development to a local network during development. It works just fine when our own device is in slave mode, but when we configure it as master it will never link up with the RDDRONE-T1ADAPT.

My understanding was that the adapter would toggle between master and slave until a connection is established. In our case LinkStatus is always down.

Is the adapter for sure able to work as a slave? Is there a way to force it into that role?

Thanks

Vic

0 Kudos
0 Replies