PTN3365

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PTN3365

613 Views
lab1
Contributor II

Hello.

Is PTN3365 ok to convert DP video source (no DP++)  to HDMI? We have read that to do that the device must have an active conversion protocol, and we dont really know if PTN3365 has it. Again, what we need is a doggle direct adaptor from simply DP to HDMI video.

Thanks

Labels (1)
Tags (1)
1 Reply

522 Views
lisettelozano
NXP Employee
NXP Employee

Hello Luis,

The PTN3365 is a fully-feature HDMI level shifter which is targeted for DisplayPort to HDMI adapters applications. It features low-swing self-biasing differential inputs which are compliant to the electrical specifications of DisplayPort Standard v1.2 and/or PCI Express Standard v1.1, and open-drain current-steering differential outputs compliant to DVI v1.0 and HDMI v1.4b electrical specifications. The I2C-bus channel actively buffers as well as level-translates the DDC signals for optimal capacitive isolation. PTN3365 also supports power-saving modes in order to minimize current consumption when no display is active or connected.

Have a great day,

Paulina

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos