PCF2129AT/1 INT output voltage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCF2129AT/1 INT output voltage

Jump to solution
1,022 Views
thomaskofoedhan
Contributor III

What is the maximum low output voltage of the INT pin?

Kind regards

Thomas

Tags (1)
0 Kudos
1 Solution
936 Views
thomaskofoedhan
Contributor III

Hi Tomas,

I had an old datasheet (should have checked) from when the PCF2129 and PCF2129A had different datasheets, and here the datasheet for the PCF2129A version did not contain this parameter. I have now updated to the latest datasheet which covers both variants and includes this parameter.

Thomas 

View solution in original post

2 Replies
936 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Thomas,

It is 0.2 x Vdd as shown in the PCF2129 datasheet:

INT pin.JPG

Best regards,

Tomas

0 Kudos
937 Views
thomaskofoedhan
Contributor III

Hi Tomas,

I had an old datasheet (should have checked) from when the PCF2129 and PCF2129A had different datasheets, and here the datasheet for the PCF2129A version did not contain this parameter. I have now updated to the latest datasheet which covers both variants and includes this parameter.

Thomas