PCA9615 OUTPUT STAGE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA9615 OUTPUT STAGE

476 Views
brienzaemanuele
Contributor I

HI,
Is possible to have some information about the output stage of the PCA9615,
information like:
-VOL of the positive and negative output voltage in function of Load,
-Max current output
-Output series resistance.
Cattura.PNG


This is my schematics, for improve the noise rejection i have decreased the pullup resistance to 200 ohm, but the output seems saturated and DP reach a voltage significantly greater than 0V and DM reach a voltage significantly smaller than 5V.

pastedImage_2.png

Thanks, Best regards.

Tags (1)
0 Kudos
1 Reply

424 Views
guoweisun
NXP TechSupport
NXP TechSupport

HI

All of DSDAP/M,DSCLP/M parameters showing in datasheet page17 Table5,except that there is no others.

Also don't suggest to use 200ohm instead of 600ohm in your circuit!

0 Kudos