NXP KEA64的PTA2和PTA3原来是配置成I2C0的,如何改配成UART0 ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NXP KEA64的PTA2和PTA3原来是配置成I2C0的,如何改配成UART0 ?

550 次查看
cnubsq
Contributor II

如题

在datasheet中找到如下信息,但不知调用哪个接口去设置?谢谢!

cnubsq_4-1664525954008.png

 

cnubsq_1-1664525900328.png

 

 

 

0 项奖励
回复
1 回复

531 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi cnubsq,

请参考UART0 not working with KE06里的答案。


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------