Hello,
I have a question about the power supply of the Level translator NTB0104/NTB0102.
I would like to use NTB0104 as bi-directional Buffer of the SPI communication line.
In that case, can I use the power supply of NTB0104 VCCA/VCCB in the same voltage?
e.g. VCC(A)=VCC(B)=3.3v
Thanks for your support.
It can't work as buffer,please follow link for buffer selection:
I²C-Bus Repeaters/Hubs/Extenders | 1 MHz up to 540 pF | NXP Semiconductors
If the voltages are equal why do you use this level shifter?
Hello
I am thinking about the following connection.
Arduino DUE(3.3v SPI) --->
+------ Buffer(NTB0104) --- 3.3v SPI Device
+------ LevelShifter(NTB0104) --- 5v SPI Device
+------ LevelShfter(NTB0104) --- 5v SPI Device
*Each device is away about 20cm.
Buffer is necessary for ArduinoDUE because a SPI interface is weaker than ArduinoUNO. and I want to take the system which reduced the kinds of a device to use.
Thanks.
Can you use the PCA9519 for replace!