MC12311 use

取消
显示结果 
搜索替代 
您的意思是: 
已解决

MC12311 use

跳至解决方案
529 次查看
steveh
Contributor II

Is anyone using the MC12311 successfully?  We cannot receive valid packets at all.  Transmitter is sending complete packets and receiver RSSI responds correctly.  SyncAddressMatch and correct CRC are never set.  Receiver RegOpMode is fixed at $10 but the IRQ flags show RxReady toggling on and off.  Should it keep switching on and off like that even when there is no mode switching?

0 项奖励
1 解答
293 次查看
steveh
Contributor II

Most of these "bugs" have a simple solution and so did this one.  It needed just a couple of bytes in the right place.

 

 

在原帖中查看解决方案

0 项奖励
3 回复数
293 次查看
georgepeterson
Contributor II

I am... at least so far.

I have two MC12311 evaluation boards and am able to make them communicate flawlessly. My end goal, however, is to use one of them in a TPMS system with an FXTH87 transmitting and I'm still working on some technical hurdles.

0 项奖励
293 次查看
georgepeterson
Contributor II

p.s. I do realize this is an old thread but my experiences are current and hopefully a reply here will initiate more discussion.

0 项奖励
294 次查看
steveh
Contributor II

Most of these "bugs" have a simple solution and so did this one.  It needed just a couple of bytes in the right place.

 

 

0 项奖励