Low power consumptions i.mx8 series processor for Medical applications design

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Low power consumptions i.mx8 series processor for Medical applications design

118件の閲覧回数
anusha57
Contributor I

Hi ,

 

We are looking for low power consumption i.MX8 series processor for your custom design.

below is the power requirements.

  • Input High Voltage: 17V
  • Input Low Voltage: 10V
  • Nominal Voltage: 12V or 16V
  • Max Power draw: 500mA @ 12V or 6W (Target)
  • Low Power Mode: ≤5mA @ 12V or 60mW (Target)

Please suggest suitable processor and share the power consumptions details.

0 件の賞賛
1 返信

97件の閲覧回数
Chavira
NXP TechSupport
NXP TechSupport

Hi @anusha57!

Thank you for contacting NXP Support!

 

You can check the power consumption of the next processors in their Application notes.

 

The next processors are designed with different features, please check the features of each one by following the link:

https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/i-mx-applications-proces...

 

iMX8MN UL

https://www.nxp.com/docs/en/application-note/AN13367.pdf

 

iMX8MN

https://www.nxp.com/docs/en/application-note/AN12778.pdf

 

iMX8ULP

https://www.nxp.com/docs/en/application-note/AN13914.pdf

 

Best Regards!

Chavira

0 件の賞賛