LX2160A fall back option for golden image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LX2160A fall back option for golden image

Jump to solution
377 Views
Akhildev
Contributor I

Hi,

We would like to know whether there is any by default option in LX2160 processor for automatic fallback of boot image to a recovery image in case of errors while booting. Should we keep an additional flash or is it doable with a single flash chip.

Thanks

0 Kudos
1 Solution
353 Views
yipingwang
NXP TechSupport
NXP TechSupport

There is no this option in LX2160 processor for automatic fallback of boot image to a recovery image.

It's better to keep the alternate bank flash or SD boot.

View solution in original post

0 Kudos
2 Replies
354 Views
yipingwang
NXP TechSupport
NXP TechSupport

There is no this option in LX2160 processor for automatic fallback of boot image to a recovery image.

It's better to keep the alternate bank flash or SD boot.

0 Kudos
350 Views
Akhildev
Contributor I

Thanks for the reply

0 Kudos