LS1028A Power Supply

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LS1028A Power Supply

488 Views
Rashmita
Contributor I

I m using LS1028A Layerscape Processor for my project. I need some clarifications regarding power section of the processor.

1)I m not using USB,DisplayPort feature ..Do i need to put power supply to those power supply pins??

2)Do i need to put Filtering circuit to PIXEL_DVDD and AVDD_PIXEL pins even if i m not using DP??

 

Kindly suggest what to do with the above unused pins

0 Kudos
1 Reply

481 Views
ufedor
NXP Employee
NXP Employee

1) Refer to the AN12028 - QorIQ LS1028A Design Checklist, Table 3. Power and ground pin termination checklist (and notes after the table).

DP supplies have to be applied for the LS1028A even if DP is not used.

2) The filtering circuits are not needed in this case.

0 Kudos