KIT-HGDRONEK66 Maximum payload

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KIT-HGDRONEK66 Maximum payload

571 Views
sfurman
Contributor I

Is there a documented maximum payload weight for the KIT-HGDRONEK66 drone kit?

0 Kudos
1 Reply

562 Views
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi @sfurman, I hope you're doing well

There's no exact value for the weight that the drone can carry, as it will depend on different factors like the motors used and the amount of them, propeller size, the frame, etc.

The NXP KIT-HGDRONEK66 drone kit is highly customizable and can be adapted to house more powerful motors or other modifications to be able to lift heavier weight.

We've compiled an additional list of recommendations and suggestions to increase this payload capacity in the GitBook page for the KIT-HGDRONEK66, here.

Please let me know if you need any more information.

Best regards,
Sebastian

0 Kudos