JN-AN-1244 Compilation problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

JN-AN-1244 Compilation problem

2,560 次查看
aaronye
Contributor I

I use MCUXpressoIDE_11.4.1_6260 to compile the project JN-AN-1244 and modify the makefile chose chip JN5189,TOOLCHAIN_DIR_PATH  modify MCUXpressoIDE_11.3.0_5222,As follows

###############################################################################
#User definable make parameters that may be overwritten from the command line

# Set specific chip (choose one)
#JENNIC_CHIP ?= K32W061
#JENNIC_CHIP ?= K32W041A
#JENNIC_CHIP ?= K32W041AM
#JENNIC_CHIP ?= K32W061
#JENNIC_CHIP ?= K32W041
JENNIC_CHIP ?= JN5189
#JENNIC_CHIP ?= JN5188

TOOLCHAIN_DIR_PATH = ../../../../../MCUXpressoIDE_11.3.0_5222/ide/tools

 

JENNIC_MAC_PLATFORM is SOC
Creating folders...

when I click build, The following error occurred:

 

Compiling ../../../Common_Light/Source/app_main.c into ../../../Binaries/ExtendedColorLight_GpProxy_OM15081/obj/app_main.o ...
../../../../../MCUXpressoIDE_11.3.0_5222/ide/tools/bin/arm-none-eabi-gcc -c -o ../../../Binaries/ExtendedColorLight_GpProxy_OM15081/obj/app_main.o -DSINGLE_CHANNEL=0 -DDEBUG_ENABLE -DMK_USE_POSITIVE_PWM=TRUE -DRTOS -DOM15081 -DgClkUseFro32K=1 -DgPWR_UseAlgoTimeBaseDriftCompensate=1 -DgClkRecalFro32K=0 -DAPP_LOW_POWER_API -DDBG_ENABLE -DPRINTF_ADVANCED_ENABLE -DDEBUG_APP -DDEBUG_START_UP -DDEBUG_LIGHT_NODE -DDEBUG_JOIN -DDEBUG_COMMISSION -DDEBUG_EXCEPTIONS -DDEBUG_APP_NTAG -DExtendedColorLight -DGP_PROXY_BASIC_DEVICE -DGP_CERITIFICATION_TEST -DCLD_GREENPOWER -DPDM_USER_SUPPLIED_ID -DNXP_HARDWARE -DBUTTON_MAP_OM15081 -DEMBEDDED -DUSER_VSR_HANDLER -DCOLORLIGHT -DRGB -DJN518x=5189 -DJN5189=5189 -DJENNIC_CHIP_NAME=_JN5189 -DJENNIC_CHIP_FAMILY_NAME=_JN518x -D__JN518X__ -DCPU_JN518X -std=gnu99 -DCORE_M4 -D__CODE_RED -fno-common -fmessage-length=0 -fno-builtin -mcpu=cortex-m4 -mthumb -fomit-frame-pointer -Os -fshort-enums -Wall -Wpacked -fdata-sections -ffunction-sections -DWATCHDOG_ALLOWED -fno-lto -DLITTLE_ENDIAN_PROCESSOR -DJENNIC_HW_BBC_RXINCCA=1 -DJENNIC_HW_BBC_DMA=1 -DJENNIC_HW_BBC_ISA=0 -DJENNIC_SW_EXTERNAL_FLASH=0 -DUART_BACKWARDS_COMPATIBLE_API=1 -DRXPOWERADJUST_SUPPORT -I../board -I../../../../../SDKPackages/JN5189DK6/CMSIS/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/boards/jn5189dk6 -I../../../../../SDKPackages/JN5189DK6/boards/jn5189dk6 -I../../../../../SDKPackages/JN5189DK6/components/serial_manager -I../../../../../SDKPackages/JN5189DK6/components/uart -I../../../../../SDKPackages/JN5189DK6/devices -I../../../../../SDKPackages/JN5189DK6/devices/JN5189 -I../../../../../SDKPackages/JN5189DK6/devices/JN5189/drivers -I../../../../../SDKPackages/JN5189DK6/devices/JN5189/utilities/debug_console -I../../../../../SDKPackages/JN5189DK6/devices/JN5189/utilities/str -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Common -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/ieee-802.15.4/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/ieee-802.15.4/uMac/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/ieee-802.15.4/mMac/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/XCVR/DK6 -DJENNIC_CHIP=JN5189 -DJENNIC_CHIP_JN5189 -DJENNIC_CHIP_FAMILY=JN518x -DJENNIC_CHIP_FAMILY_JN518x -DJENNIC_STACK_MAC -DJENNIC_MAC_MiniMacShim -Wall -Wunreachable-code -DEMBEDDED -DosNumberOfSemaphores=0 -DosNumberOfMutexes=0 -DosNumberOfMessageQs=0 -DosNumberOfMessages=0 -DosNumberOfEvents=0 -DgMainThreadStackSize_c=0 -DgMainThreadPriority_c=0 -DgTaskMultipleInstancesManagement_c=0 -DFSL_OSA_BM_TIMER_CONFIG=FSL_OSA_BM_TIMER_SYSTICK -DDBG_ENABLE -DDEBUG_ENABLE -DENABLE_RAM_VECTOR_TABLE -DSDK_DEVICE_FAMILY=JN5189 -DgPWRM_Support=1 -DgSupportBle=0 -DcPWR_FullPowerDownMode=1 -DZIGBEE_USE_FRAMEWORK=1 -DPDM_USER_SUPPLIED_ID -DPDM_NO_RTOS -DZPS_APL_OPT_SINGLE_INSTANCE -DOTA_NO_CERTIFICATE -DPLME_SAP -DZBPRO_DEVICE_TYPE_ZCR -DBDB_SUPPORT_NWK_STEERING -DBDB_SUPPORT_TOUCHLINK -DBDB_SUPPORT_FIND_AND_BIND_TARGET -I../../../Common_Light/Source -I../../../ExtendedColorLight/Source -I../../../Common_Light/Source/board -I../../../Common_Light/Source/DriverBulb -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/SerialMAC/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZPSMAC/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZPSNWK/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZPSTSV/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZigbeeCommon/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZPSAPL/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/PWRM/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/PDUM/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Lists -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/PDM/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/DBG/Include -I../../../../../SDKPackages/JN5189DK6/boards/jn5189dk6 -I../../../../../SDKPackages/JN5189DK6/devices/JN5189 -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/DebugExceptionHandlers_jn518x/src/../inc -I/../Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/DebugFifo/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/OSAbstraction/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/FunctionLib -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/SecLib -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/RNG/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/MemManager/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Panic/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Messaging/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/OtaSupport/Source/../Interface/ -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/TimersManager/Interface/ -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Flash/Internal -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Flash/External/Source/../Interface/ -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Flash/Internal/../Interface/ -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Panic/Interface/ -I../../../../../SDKPackages/JN5189DK6/devices/JN5189/drivers -I../../../../../SDKPackages/JN5189DK6/components/serial_manager/ -I../../../../../SDKPackages/JN5189DK6/components/uart -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/LowPower/Source/jn5189dk6/../../Interface/jn5189dk6 -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/GPIO -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCIF/Source -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCIF/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/General/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/General/Source -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/MeasurementAndSensing/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/Lighting/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/HVAC/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/Closures/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/SecurityAndSafety/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/SmartEnergy/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/OTA/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/Commissioning/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/ApplianceManagement/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/GreenPower/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Devices/ZHA/Generic/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Devices/ZLO/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Devices/ZGP/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Source/Common -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Source/NwkSteering -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Source/TouchLink -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Source/FindAndBind ../../../Common_Light/Source/app_main.c -MD -MF ../../../Binaries/ExtendedColorLight_GpProxy_OM15081/obj/.d -MP
process_begin: CreateProcess(NULL, ../../../../../MCUXpressoIDE_11.3.0_5222/ide/tools/bin/arm-none-eabi-gcc -c -o ../../../Binaries/ExtendedColorLight_GpProxy_OM15081/obj/app_main.o -DSINGLE_CHANNEL=0 -DDEBUG_ENABLE -DMK_USE_POSITIVE_PWM=TRUE -DRTOS -DOM15081 -DgClkUseFro32K=1 -DgPWR_UseAlgoTimeBaseDriftCompensate=1 -DgClkRecalFro32K=0 -DAPP_LOW_POWER_API -DDBG_ENABLE -DPRINTF_ADVANCED_ENABLE -DDEBUG_APP -DDEBUG_START_UP -DDEBUG_LIGHT_NODE -DDEBUG_JOIN -DDEBUG_COMMISSION -DDEBUG_EXCEPTIONS -DDEBUG_APP_NTAG -DExtendedColorLight -DGP_PROXY_BASIC_DEVICE -DGP_CERITIFICATION_TEST -DCLD_GREENPOWER -DPDM_USER_SUPPLIED_ID -DNXP_HARDWARE -DBUTTON_MAP_OM15081 -DEMBEDDED -DUSER_VSR_HANDLER -DCOLORLIGHT -DRGB -DJN518x=5189 -DJN5189=5189 -DJENNIC_CHIP_NAME=_JN5189 -DJENNIC_CHIP_FAMILY_NAME=_JN518x -D__JN518X__ -DCPU_JN518X -std=gnu99 -DCORE_M4 -D__CODE_RED -fno-common -fmessage-length=0 -fno-builtin -mcpu=cortex-m4 -mthumb -fomit-frame-pointer -Os -fshort-enums -Wall -Wpacked -fdata-sections -ffunction-sections -DWATCHDOG_ALLOWED -fno-lto -DLITTLE_ENDIAN_PROCESSOR -DJENNIC_HW_BBC_RXINCCA=1 -DJENNIC_HW_BBC_DMA=1 -DJENNIC_HW_BBC_ISA=0 -DJENNIC_SW_EXTERNAL_FLASH=0 -DUART_BACKWARDS_COMPATIBLE_API=1 -DRXPOWERADJUST_SUPPORT -I../board -I../../../../../SDKPackages/JN5189DK6/CMSIS/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/boards/jn5189dk6 -I../../../../../SDKPackages/JN5189DK6/boards/jn5189dk6 -I../../../../../SDKPackages/JN5189DK6/components/serial_manager -I../../../../../SDKPackages/JN5189DK6/components/uart -I../../../../../SDKPackages/JN5189DK6/devices -I../../../../../SDKPackages/JN5189DK6/devices/JN5189 -I../../../../../SDKPackages/JN5189DK6/devices/JN5189/drivers -I../../../../../SDKPackages/JN5189DK6/devices/JN5189/utilities/debug_console -I../../../../../SDKPackages/JN5189DK6/devices/JN5189/utilities/str -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Common -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/ieee-802.15.4/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/ieee-802.15.4/uMac/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/ieee-802.15.4/mMac/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/XCVR/DK6 -DJENNIC_CHIP=JN5189 -DJENNIC_CHIP_JN5189 -DJENNIC_CHIP_FAMILY=JN518x -DJENNIC_CHIP_FAMILY_JN518x -DJENNIC_STACK_MAC -DJENNIC_MAC_MiniMacShim -Wall -Wunreachable-code -DEMBEDDED -DosNumberOfSemaphores=0 -DosNumberOfMutexes=0 -DosNumberOfMessageQs=0 -DosNumberOfMessages=0 -DosNumberOfEvents=0 -DgMainThreadStackSize_c=0 -DgMainThreadPriority_c=0 -DgTaskMultipleInstancesManagement_c=0 -DFSL_OSA_BM_TIMER_CONFIG=FSL_OSA_BM_TIMER_SYSTICK -DDBG_ENABLE -DDEBUG_ENABLE -DENABLE_RAM_VECTOR_TABLE -DSDK_DEVICE_FAMILY=JN5189 -DgPWRM_Support=1 -DgSupportBle=0 -DcPWR_FullPowerDownMode=1 -DZIGBEE_USE_FRAMEWORK=1 -DPDM_USER_SUPPLIED_ID -DPDM_NO_RTOS -DZPS_APL_OPT_SINGLE_INSTANCE -DOTA_NO_CERTIFICATE -DPLME_SAP -DZBPRO_DEVICE_TYPE_ZCR -DBDB_SUPPORT_NWK_STEERING -DBDB_SUPPORT_TOUCHLINK -DBDB_SUPPORT_FIND_AND_BIND_TARGET -I../../../Common_Light/Source -I../../../ExtendedColorLight/Source -I../../../Common_Light/Source/board -I../../../Common_Light/Source/DriverBulb -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/SerialMAC/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZPSMAC/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZPSNWK/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZPSTSV/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZigbeeCommon/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZPSAPL/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/PWRM/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/PDUM/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Lists -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/PDM/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/DBG/Include -I../../../../../SDKPackages/JN5189DK6/boards/jn5189dk6 -I../../../../../SDKPackages/JN5189DK6/devices/JN5189 -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/DebugExceptionHandlers_jn518x/src/../inc -I/../Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/DebugFifo/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/OSAbstraction/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/FunctionLib -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/SecLib -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/RNG/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/MemManager/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Panic/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Messaging/Interface -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/OtaSupport/Source/../Interface/ -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/TimersManager/Interface/ -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Flash/Internal -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Flash/External/Source/../Interface/ -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Flash/Internal/../Interface/ -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/Panic/Interface/ -I../../../../../SDKPackages/JN5189DK6/devices/JN5189/drivers -I../../../../../SDKPackages/JN5189DK6/components/serial_manager/ -I../../../../../SDKPackages/JN5189DK6/components/uart -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/LowPower/Source/jn5189dk6/../../Interface/jn5189dk6 -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/framework/GPIO -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCIF/Source -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCIF/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/General/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/General/Source -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/MeasurementAndSensing/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/Lighting/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/HVAC/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/Closures/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/SecurityAndSafety/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/SmartEnergy/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/OTA/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/Commissioning/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/ApplianceManagement/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Clusters/GreenPower/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Devices/ZHA/Generic/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Devices/ZLO/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/ZCL/Devices/ZGP/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Include -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Source/Common -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Source/NwkSteering -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Source/TouchLink -I../../../../../SDKPackages/JN5189DK6/middleware/wireless/zigbee/BDB/Source/FindAndBind ../../../Common_Light/Source/app_main.c -MD -MF ../../../Binaries/ExtendedColorLight_GpProxy_OM15081/obj/.d -MP, ...) failed.
make (e=2): 系统找不到指定的文件。

make: *** [Makefile:667: ../../../Binaries/ExtendedColorLight_GpProxy_OM15081/obj/app_main.o] Error 2
"make LIGHT=ExtendedColorLight DR=OM15081 TRACE=1 APP_NTAG_ICODE=0 OTA=0 GP_SUPPORT=1 GP_DEVICE=PROXY_BASIC -r all" terminated with exit code 2. Build might be incomplete.

20:22:26 Build Failed. 1 errors, 0 warnings. (took 1s.560ms)

Could you tell me how to solve this problem?

 

 

0 项奖励
回复
4 回复数

2,517 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

 你有没有创建这样的目录结构c:/nxp/SDKPackage,把sdk放进去,同时重命名

aa.PNG

0 项奖励
回复

2,501 次查看
aaronye
Contributor I

有创建这样一个文件夹,我用的编译器是 MCUXpressoIDE_11.4.1_6260,请问有没有文档能够告诉我如何将将JN-AN-1244 例程编译成功的? 相比JN5169 感觉这个编译器太难用了

aaronye_0-1639535531468.png

 

0 项奖励
回复

2,497 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

我是能编译通过的,应该是环境设置的有问题,看着附件再检查一下环境,确定该有的文件夹都在正确位置

0 项奖励
回复

2,473 次查看
aaronye
Contributor I

编译通过了,谢谢!

0 项奖励
回复