Does J-Flash can program 512kb in kw38

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does J-Flash can program 512kb in kw38

跳至解决方案
1,081 次查看
jingfang
Contributor IV

KW38 is 256kb program flash + 256kb flexnvm.

When use J-Flash erase show : selected data does not fit into selected flash sectors.

How should I slove it?

be98c484-388b-47b1-a733-1a440b8ad4a5.jpgc7c8add8-f8e0-45da-acd8-d4477ca9f9b5.jpg

0 项奖励
1 解答
1,011 次查看
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

I apologize for the inconvenience this might cause you, could you please contact SEGGER for more information about this inquiry?

Regards,
Eduardo.

在原帖中查看解决方案

0 项奖励
7 回复数
1,058 次查看
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @jingfang,

Hope you are doing well.

Just to confirm, are you using a custom board or is it a FRDM board?

Are you trying to perform an Erase Sector or is it Erase Chip (Manual programming)? Does this error occur if you try to program a binary file?

By any chance, have you modified the Flash setting? Could you please share a screenshot of your Flash settings (Options tab > Project Settings… > Flash)?

Please consider doing some tests with J-Flash Lite and JLink Commander (Jlink.exe), just to confirm the behavior that your application presents. You can find the corresponding User Manuals inside SEGGER > JLink > Doc > Manuals.

Regards,
Eduardo.

0 项奖励
1,053 次查看
jingfang
Contributor IV

I test J-Flash V7.70 with demo board KW38,the problem points remain.(IDE GUI FLASH TOOL is OK).

J-Flash set as follows:

7922c2c9-85bd-4cac-a270-44f5a42779b4.jpg774015f2-2173-48f5-985f-4ca588995770.jpg

The bin file size is 520KB.

0 项奖励
1,037 次查看
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

Just to confirm, what is the programmer/debug probe you are using (for example JLink base, JLink Pro, JLink Plus...)? I am still trying to reproduce this scenario on my side.

Could you please try flashing a binary file with a smaller size? Please consider doing a mass erase to the flash memory using the GUI Flash Tool before programming. After this, try to flash a smaller binary.

Regards,
Eduardo.

0 项奖励
1,030 次查看
jingfang
Contributor IV

small size bin is ok,I split the 512KB bin into 256+256KB,it is ok.

Jlink as follows:

27d9b417-8dcd-4857-a23f-6f22e3d2afb0.jpg

0 项奖励
1,026 次查看
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

Does this mean that you found a workaround and the problem is now solved? Could you please confirm this?

Regards,
Eduardo.

0 项奖励
1,022 次查看
jingfang
Contributor IV

I found a solution, but this one requires splitting the bin file. 

I wonder, is there a way to do this without splitting the bin file?

0 项奖励
1,012 次查看
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

I apologize for the inconvenience this might cause you, could you please contact SEGGER for more information about this inquiry?

Regards,
Eduardo.

0 项奖励