DCD-LZ breakout board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DCD-LZ breakout board

1,252 Views
Evangelos_Liolis
Contributor I

Hi all,

 

is there a way that I can purchase the NXP DCD-LZ breakout board?I can't seem to find a link.

5 Replies

1,048 Views
iaingalloway
NXP Employee
NXP Employee

Sorry to say - at the moment it is included only with the UCANS32K1SIC boards and also the HoverGames drone and RDDRONE-FMUK66

The board only provides a breakout connection to a debugger SWD/SWO lines and a separate USB-UART.  It is not too difficult to buy a JST-GH connector and wire it manually to an adapter cable.
The pinout is shown here:
https://nxp.gitbook.io/hovergames/rddrone-fmuk66/connectors/debug-interface-dcd-lz/dcd-lz-breakout-b...


 

0 Kudos

1,188 Views
DaveNXP
Contributor III

I don't know if you can buy it but as far as I know you can design the board with the schematic resource. And if you have a 3D printer, printing the case, which is also provided. I attach the two links with schematic and 3D design.

https://nxp.gitbook.io/hovergames/rddrone-fmuk66/connectors/debug-interface-dcd-lz/dcd-lz-breakout-b...

https://www.thingiverse.com/thing:2928573

 

0 Kudos

1,190 Views
safedryverdubai
Contributor I

That agree. SafeDryver would really appreciate it if you could find a way to get the breakout board.

safedryver.com
0 Kudos

1,193 Views
DaveNXP
Contributor III

Me too. If you find any way to get the beakout board I would really appreciate it.

0 Kudos

1,228 Views
lmiles-sosub
Contributor II

I am also looking to purchase the board. If you find any information can you please share it. Thanks.

0 Kudos