Computing Power dissipation (current consumption) of microcontroller MPC5643L according to the datasheet???

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Computing Power dissipation (current consumption) of microcontroller MPC5643L according to the datasheet???

跳至解决方案
920 次查看
rasoulmobasheri
Contributor I

Hello to all,

Could someone help me with the Current consumption computation of the micro controller MPC5643L ?

my guess is something like : TotalPowerConsumption = RunModePower + Sleep × deepSleepModePower and it should be some integral shape equation since it won't be a linear and dependent on our time period. I don't know that how can I compute this current with regards to the data sheet.

any idea and answer would be appreciated. Thanks in Advance.

Regards

Ras

0 项奖励
回复
1 解答
600 次查看
LPP
NXP Employee
NXP Employee

Typical purposes of current consumption computation are to scale power supply or thermal management.

1.

It doesn't matter if the device is sleeping most time or not. Anyway, power supply must be able to provide maximum current consumed by the device.

HV supply should scaled at max(IDD_LV_FULL + IDD_LV_PLL + IDD_HV_xx) current.

80 mA + 2.50 mA*fCPU[MHz] + 10ma + 3ma + 3.5ma + 4ma + 10ma = 410.5ma @ 3.3V, 150'C, 120MHz

Recommended supply current ~450ma.

2.

Thermal management. Use typical current  consumption characteristics.

If LV internal ballast transistor is used:

P_tot = typ (IDD_LV_FULL + IDD_LV_PLL + IDD_HV_xx) * 3.3V

P_tot = (41 ma + 2.3 mA*fCPU[MHz] + 10ma + 3ma + 3.5ma + 4ma + 10ma)*3.3V = 1.15W @ 150'C, 120MHz

If LV external ballast transistor is used:

P_tot = typ (IDD_LV_FULL + IDD_LV_PLL)*1.32V + IDD_HV_xx * 3.3V

P_tot = (41 ma + 2.3 mA*fCPU[MHz])*1.32V + (10ma + 3ma + 3.5ma + 4ma + 10ma)*3.3 = 0.52W @ 150'C, 120MHz

3.

Power consumption estimation in HALT mode.

P_HALT = typ (IDD_LV_HALT + IDD_HV_xx) * 3.3V

P_HALT = (115ma + 30.5ma) * 3.3V = 0.48W @ 150'C, 120MHz

This estimation provides some margin since IDD_HV_xx consumption in sleep modes should be less than in full run mode.

4.

If you want to estimate average consumption in mixed sleep/run mode:

P_average = P_tot * duty + P_HALT*(1-duty)

Note. All estimations are made at Tj=150'C.


Have a great day,
Paul

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
600 次查看
rasoulmobasheri
Contributor I

Hey Paul,

that's exactly what I needed. Thanks a lot.

Cheers

Ras

0 项奖励
回复
601 次查看
LPP
NXP Employee
NXP Employee

Typical purposes of current consumption computation are to scale power supply or thermal management.

1.

It doesn't matter if the device is sleeping most time or not. Anyway, power supply must be able to provide maximum current consumed by the device.

HV supply should scaled at max(IDD_LV_FULL + IDD_LV_PLL + IDD_HV_xx) current.

80 mA + 2.50 mA*fCPU[MHz] + 10ma + 3ma + 3.5ma + 4ma + 10ma = 410.5ma @ 3.3V, 150'C, 120MHz

Recommended supply current ~450ma.

2.

Thermal management. Use typical current  consumption characteristics.

If LV internal ballast transistor is used:

P_tot = typ (IDD_LV_FULL + IDD_LV_PLL + IDD_HV_xx) * 3.3V

P_tot = (41 ma + 2.3 mA*fCPU[MHz] + 10ma + 3ma + 3.5ma + 4ma + 10ma)*3.3V = 1.15W @ 150'C, 120MHz

If LV external ballast transistor is used:

P_tot = typ (IDD_LV_FULL + IDD_LV_PLL)*1.32V + IDD_HV_xx * 3.3V

P_tot = (41 ma + 2.3 mA*fCPU[MHz])*1.32V + (10ma + 3ma + 3.5ma + 4ma + 10ma)*3.3 = 0.52W @ 150'C, 120MHz

3.

Power consumption estimation in HALT mode.

P_HALT = typ (IDD_LV_HALT + IDD_HV_xx) * 3.3V

P_HALT = (115ma + 30.5ma) * 3.3V = 0.48W @ 150'C, 120MHz

This estimation provides some margin since IDD_HV_xx consumption in sleep modes should be less than in full run mode.

4.

If you want to estimate average consumption in mixed sleep/run mode:

P_average = P_tot * duty + P_HALT*(1-duty)

Note. All estimations are made at Tj=150'C.


Have a great day,
Paul

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复