'AMP_BLP35M805_V1p02/AMP_BLQC0801_001' model required

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

'AMP_BLP35M805_V1p02/AMP_BLQC0801_001' model required

719 Views
UshaPerumal
Contributor I

Hi

I am simulating in ads, the  model  used is  AMP_BLP35M805_V1p02. I am getting  the following error. 

Simulation Messages

Warning detected by hpeesofsim during netlist parsing.
Model `AMP_BLQC0801_001.MDL_6MM' (defined in file 'AMP_BLP35M805_V1p02/AMP_BLQC0801_001' around line 3): `SPEAR104T' is an undefined primitive device.
Error detected by hpeesofsim during netlist flattening.
`AMP_BLQC0801_001.Qcell' is an instance of an undefined model `MDL_6MM'.

Status / Summary


hpeesofsim (*) 512.update2.0 Feb 27 2020, MINT version 5
(64-bit windows built: Thu Feb 27, 2020 19:34:00 +0000)
--------------------
Simulation terminated due to error.
--------------------

 

Kindly suggest us to solve this problem.

0 Replies