Very special antenna design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Very special antenna design

615 Views
jof
Contributor I

My task is to design a antenna to read a mifare tag.

I try to describe the application:

Imagine a credit card shaped tag, but way smaller (25mm long, 11mm high, 3mm thick). This tag travels trough a tube with 15mm ID. This limits the turn of the card to the Z-Axis. So seen from a 0 degree point, the card can have any particular degree of turn from 0-359 degree.

At the postion of the reader, the card will be stopped, but cannot brought to a defined angle.

The reader antenna must be placed around the tube and has to be able to read the tag in any particular angle of Z.

Which antenna type/shape would be reccomended for this application? Maybe someone here knows about a similar application design.

Any help is appreciated

Tags (1)
0 Kudos
2 Replies

517 Views
jof
Contributor I

I'm using the CLRC663

0 Kudos

517 Views
jimmychan
NXP TechSupport
NXP TechSupport

which chip are you using?

0 Kudos