PR533 and PICC not 14443-4-compliant

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PR533 and PICC not 14443-4-compliant

495 Views
doumiaoya
Contributor I

Can PR533 find the PICC which is not ISO14443-4-compliant?

Is there any way to opration the PICC?

pastedImage_1.png

0 Kudos
1 Reply

443 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Haitao,

   See below, please!

-------------------------------

PR533 Reader/writer functionality compatible with ISO/IEC 14443 A&B, MIFARE™, FeliCa, and NFC Forum tag types (Jewel, MIFARE Ultralight, FeliCa, FeliCa lite, MIFARE DESFire), and supports I-class (Picopass B type modulation)

--------------------------------

It means PR533 supports TAG Type 1, 2,3,4.  so if your PICC support one of them, it is no problem to operate it.

Have a nice day!

BR,

weidong

0 Kudos