Can PR533 find the PICC which is not ISO14443-4-compliant?
Is there any way to opration the PICC?
Hi Haitao,
See below, please!
-------------------------------
PR533 Reader/writer functionality compatible with ISO/IEC 14443 A&B, MIFARE™, FeliCa, and NFC Forum tag types (Jewel, MIFARE Ultralight, FeliCa, FeliCa lite, MIFARE DESFire), and supports I-class (Picopass B type modulation)
--------------------------------
It means PR533 supports TAG Type 1, 2,3,4. so if your PICC support one of them, it is no problem to operate it.
Have a nice day!
BR,
weidong