PN7462AUHN/C300E and PN7462AUHN/C300Y

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN7462AUHN/C300E and PN7462AUHN/C300Y

1,695件の閲覧回数
khalid_anindyag
Contributor I

Hello.

What is the difference between PN7462AUHN/C300E and PN7462AUHN/C300Y? Is the footprint and functionalities same? 

Please kindly answer ASAP. Thank you.

Best regards,

Khalid

タグ(2)
0 件の賞賛
返信
2 返答(返信)

1,561件の閲覧回数
aaronjimison
Contributor I

Ivan,

Can you tell me what the /C300 and /C200 call out?

1,561件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

The difference between these two is basically the packing. The part number ending in C300E comes in tray (please see image below), while the one ending in C300Y is available in REEL as mentioned in the image below:

pastedImage_1.png

Have a nice day.

BR,

Ivan.