NT2H1611G0DA8 - What Are MOA8 Dimensions?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NT2H1611G0DA8 - What Are MOA8 Dimensions?

999 Views
jcwest
Contributor I

Hello,

Can I get the dimensions of the NT2H1611G0DA8 part?  Supposed to be in an MOA8 package that is allegedly defined here:

https://www.nxp.com/docs/en/package-information/SOT500-4.pdf

except that's incomplete - even says:

"For unspecified dimensions see PLLMC-drawing given in the subpackage code." - what and where is the subpackage code?

Can you please post the package dimensions, in exhaustive detail, of the MOA8 package?

Thanks!
John

 

0 Kudos
2 Replies

986 Views
jcwest
Contributor I

fangfang,

I bought some off of Mouser and I need an NDA to get dimensions of the package?  Really?

https://www.mouser.com/ProductDetail/nxp/nt2h1611g0da8j/?qs=gH1BdSMZm8U5sTTCTe%252bb5Q%3D%3D&country...

Why can't I get the device package dimensions?

Can you just tell me if the La pad distance from the Lb pad is approx. 6mm?

Thanks,
johnwest

 

 

0 Kudos

989 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

This information is in docstore, please access to the following document in docstore.
Package drawing Dr194641 - MOA8 Package Drawing 3312 062 56531 (4.1) If the customer has the NDA.

 

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos