NFC Antenna Tuning using calibration coil

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC Antenna Tuning using calibration coil

Jump to solution
696 Views
hengma
Contributor I

Hi,

 

I have a question related to the antenna tuning process of RFID readers using CLRC663. I noticed that all application notes use VNA to measure the impedance at the Tx ports of the chipset. May I know if there is an indirect way to tune the antenna? For example, can we place a calibration coil on the reader and measure the voltage from the calibration coil? A high-impedance probe is used to measure the voltage from the calibration coil. The antenna is tuned using a variable capacitor and is considered to be well-tuned once the maximum voltage from the calibration coil is obtained. May I know if it is feasible?

 

Thanks,

 

Heng

 

 

0 Kudos
1 Solution
647 Views
KellyLi
NXP TechSupport
NXP TechSupport

Hello @hengma 

Thanks for contacting us and using the NXP products.

Your approach sounds feasible, but NXP has no such precedent, so it is difficult to give you relevant advice. It is still recommended that you use the method recommended by NXP to achieve it.

BR

kelly

View solution in original post

2 Replies
648 Views
KellyLi
NXP TechSupport
NXP TechSupport

Hello @hengma 

Thanks for contacting us and using the NXP products.

Your approach sounds feasible, but NXP has no such precedent, so it is difficult to give you relevant advice. It is still recommended that you use the method recommended by NXP to achieve it.

BR

kelly

578 Views
hengma
Contributor I
Thanks for that. Understood.
0 Kudos