Mifare Ultralight C - Changing default password and protecting page address

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Mifare Ultralight C - Changing default password and protecting page address

Mifare Ultralight C - Changing default password and protecting page address

pastedImage_101.png

Hello NFC community,
MIFARE® Ultralight-based tickets offer an ideal solution for low-cost, high-volume applications such as public transport, loyalty cards and event ticketing. They serve as a perfect contactless replacement for magnetic stripe, barcode, or QR-code systems. The introduction of the contactless MIFARE Ultralight® ICs for limited-use applications can lead to reduced system installation and maintenance costs. As you may know the MIFARE family has the Ultralight C tag which is a contactless IC supporting 3DES cryptography is mostly used in limited use applications such smart ticketing, this tag complies with ISO 14443-3 type A and it is defined as type 2 tag, in this document I want to show you the procedure to change the default key to a custom key also to protect certain areas in the tag so the authentication is needed to perform a read or write operation.

---------------------------------------------------------------------------------------------------

For this document I used :

---------------------------------------------------------------------------------------------------

Information

  • Old Key : 49454D4B41455242214E4143554F5946
  • New Key : 88776655443322117766554433221199
  • Data sheet

----------------------------------------------------------------------------------------------------

  • First we start with the procedure to activate the tag and the anticollision procedure explained in the ISO/IEC 14443-3.

Command Direction

  •    ">" this direction is command send from PCD (Reader) to PICC(Ultralight c)
  •    "<" this direction is command send from PICC (Ultralight c) to PCD (Reader)
  •    "=" Prepare this command before sending

Command

 

Data message

REQA =  Request Command, Type A

26

ATQA = Answer To Request, Type A 

4400

SEL + NVB = SEL (Select code for cascade level ) 93, NVB (Number of Valid bits) 20

9320

ANTICOLLISION START

8804598356

 

93708804598356

SAK (Select Acknowledge) = indicates additional cascade level

x04

 

9520

 

E1ED2580A9

 

9570E1ED2580A9

 

x00

UID = 045983E1ED2580

 ** the following procedure is explained in section 7.5.5 from the datasheet**

Command

 

Data message

Authenticate Part 1  (command 1A)

1A00

 

AFA1ED1D682E5101422CC7

Authenticate Part 2 (command AF)

AF2970D895F186D0302970D895F186D030188AAF4DAF68C5B9

 

006BD027CEC3E04EBC6919

[AUTHENTICATED]

Then according to  section 7.5.7 of the datasheet the sections  where the 3DES key are saved are the 2C (Page 44) to the 2F (Page 47).

pastedImage_22.png

We proceed to  write our new key using the A2 (WRITE command)

Command

 

Data message

DATA = byte 07,06,05,04

=

11223344

WRITE to page 44 (2C)

A22C11223344

Positive acknowledge (ACK)

0A

DATA = byte 03,02,01,00

=

55667788

WRITE to page 45 (2D)

A22D55667788 

Positive acknowledge (ACK)

0A

DATA = byte 0F,0E,0D,0C

=

99112233

WRITE to page 46 (2E)

A22E99112233 

Positive acknowledge (ACK)

0A

DATA = byte 0B,0A,09,08

=

44556677

WRITE to page 47 (2F)

A22F44556677 

Positive acknowledge (ACK)

0A

[RESET FIELD]
[Authenticate with new key]

Command

 

Data message

Authenticate Part 1  (command 1A

1A00

 

AFFAE2EFF17FAAD69862E7

Authenticate Part 2 (command AF)

AFFD5794F2D4EA1B19FD5794F2D4EA1B196CF420CD4D9E8104

 

0030922228601939B8FA18

[AUTENTICATED WITH NEW KEY]

we proceed to define from which sector the authentication is needed in order to read or write, to do this we use a write command to the AUTH0 (AUTH0 defines the page address from which the authentication is required. Valid address values for byte AUTH0 are from 03h to 30h.)

the AUTH0 is located on the section 2A please check table 5 from #datasheet.

pastedImage_29.png

**for this example we will define that from page 6 (06) we will need authentication to perform a read or write operation**

Command

 

Data message

WRITE command (A2) to AUTH0 (2A) from page 6 (06)

A22A06000000

Positive acknowledge (ACK)

0A

Now the Read capabilities from page 06  require an Authentication in order to be read or written.

Hope you find this document useful to get a better understanding of the behavior of the Ultralight C and how its security features can help you in your applications.

Have a great day!

BR

Jonathan

标签 (1)
无评分
版本历史
最后更新:
‎09-24-2018 12:44 PM
更新人: